Skip to content Skip to navigation
Resources About MyPortal Login
Edit Entry
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
Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking

By Audience

School Solutions
School Solutions
Student Solutions
Student Solutions
Workforce Training
Workforce Training
Education Sales Education Partners
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Articles
  4. ›
  5. How Robotics Is Evolving to Create More Adaptable Automation in Modern Manufacturing
A white FANUC collaborative robot arm working at a metal bench beside a handheld teach pendant with a touchscreen interface and red emergency stop button.

How Robotics Is Evolving to Create More Adaptable Automation in Modern Manufacturing

Modern robotics blends sensing, AI and flexible tools to enable fast changeovers and adaptable automation for evolving manufacturing demands.

Published
February 13, 2026
Last Updated
September 3, 2026
Reading Time
3 min
Share Facebook X LinkedIn Email Copied link
Geoff Dawson
Geoff Dawson
FANUC America

Manufacturers today face a production landscape defined by rapid change. Product lifecycles are shrinking, part variability is increasing, and changeovers that once happened quarterly now occur weekly—or even daily. In this environment, the traditional model of fixed, rigid automation simply doesn’t provide the flexibility companies need to stay competitive. That’s why adaptability has become one of the most important attributes in modern robotic systems.

Across industries, we’re seeing customers demand automation that can be reconfigured quickly without lengthy reprogramming or downtime. Fortunately, advances in programming tools are making this not only possible but increasingly simple. Offline simulation, graphical interfaces and template-based programming have dramatically reduced the time required to adjust robot tasks. Updates that once took hours using traditional programming styles can now be completed far faster and often without stopping production. AI tools are also showing enhancements that can allow for quicker changeovers.

Mechanical flexibility is advancing as well. Many robotic workcells now leverage automatic tool changers with standardized mechanical and electrical interfaces, allowing operators to switch between end-of-arm tools in minutes. Modular gripper systems, ranging from interchangeable fingers to vacuum modules and servo-driven mechanisms, make it easier to handle a wider range of parts without complex redesigns or calibration work.

Robots themselves are evolving to support greater adaptability. Machines today feature deeper integration of sensing technologies, including force and torque sensors that allow robots to “feel” contact and adjust accordingly. FANUC’s force-sensing capabilities, for example, enable more forgiving and precise motion during assembly, polishing and other processes that involve part variability. Likewise, embedded vision systems directly connected to the robot controller provide fast, reliable part detection—even when orientations or environmental conditions shift.

Artificial intelligence is adding an additional layer of responsiveness. By interpreting sensory data in real time, AI helps robots adapt to material differences, part tolerances and unexpected process conditions. When manual adjustments are required, AI-enabled systems can learn from those interventions and apply the corrections in future cycles.

At FANUC, improving flexibility is central to our development strategy. We’re expanding integrated sensing and simulation tools that help customers validate changes virtually before deploying them on the floor. We’re investing in open platforms, including ROS 2 connectivity, Python support and enhanced streaming motion, to give developers more freedom to build adaptive solutions. And through our work with NVIDIA on real time AI perception, we’re helping customers leverage digital twins and advanced reasoning to accelerate changeovers and optimize production.

As manufacturing continues to evolve, so must automation. By combining sensing, intelligence and open architectures, we're enabling robots that can adjust, respond and redeploy with unprecedented ease. That helps our customers drive productivity no matter how quickly their operations change.