Why a CNC Retrofit Beats Buying a New Machine Tool
When a legacy machine tool is not performing optimally, a CNC retrofit might be the key to cost savings and boosting productivity.
- Published
- Last Updated
- Reading Time
- 3 min
Machine tools are among the most vital—and costly—pieces of equipment on most shopfloors. As a significant capital investment, they must maintain their viable for many years. The good news is that once it reaches its end of use, you might be able to extend its life through a CNC retrofit by replacing its CNC, servo and spindle systems. Assuming the machine tool is mechanically sound, updating it with the latest CNC control technologies is often the most cost-effective and economically sustainable solution to enhance its overall performance.
The Benefits of CNC Retrofitting
Replacing an older control in CNC equipment allows you to avoid the high capital expenditure of purchasing a new machine tool while maximizing productivity. Here are several compelling reasons to retrofit your legacy equipment:
- Cost savings: A retrofit will cost approximately one-third to half the price of a new machine. Plus, with the additional cost savings from reduced repairs, this can significantly lower your total cost of ownership.
- Preventive maintenance: A CNC retrofit extends the operating life of your machine tool by minimizing unplanned downtime due to failures as well as improving reliability.
- Higher performance: New CNCs offer advanced, fully digital servo and spindle drives. These drives are highly integrated as a single system for increased productivity.
- Increased safety: Modern CNC systems include predictive, preventive, diagnostic and troubleshooting functions. For instance, new controls feature alert systems for process and downtime failures. Also, software like FANUC’s Dual Check Safety is built-in to protect operators, robots and tooling.
- Superior connectivity: New CNCs support high-speed Ethernet, enabling integration into IT networks. High-speed fiber optic communication paths connect intelligent feedback devices and inter-process communication.
- Forward-looking sustainability: Retrofitting helps extend the life of existing machines, keeping them working for longer to support sustainable practices and reduce unnecessary equipment waste.
- Future-proof compatibility: Standardizing on a single CNC brand optimizes operations. Operators can easily move between machines controlled by the same platform without needing extensive training. Also, if upgrading to robotic machine tending, a unified control platform can help simplify integrating advanced automation.
- Improved uptime: Advanced CNC technology and software reduce mean time to repair and lower the risk of unplanned downtime.
- Boosts production: New CNCs can reduce cycle times by as much as 50 percent with features like block look-ahead, acceleration/deceleration before and after interpolation, nano-interpolation, nano-smoothing and automatic feed rate control.
- Advanced machining functions: New CNC features, such as tool center point control and 3D Error Compensation, make 5-axis workflow as efficient as 3-axis with any adjustments made directly on the CNC.
- Energy savings: New digital drives regenerate electrical energy during the deceleration of the servo and spindle motors. Combined with the low-loss power devices and efficient machining processes provided by the CNC, electricity costs can be reduced by as much as 50 percent.
Final Thoughts
A CNC retrofit is a smart way to extend the life of legacy machine tools while saving costs. Retrofitted machines are more efficient, reliable and easier to maintain. Plus, you avoid the hassle of sourcing obsolete parts that are increasingly difficult, and sometimes impossible, to find.