Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Cobot Beveling and FANUC Machining Centers Boost Quality and Productivity for Optics Manufacturer

Cobot Beveling and FANUC Machining Centers Boost Quality and Productivity for Optics Manufacturer

Sydor Optics automated beveling with a FANUC cobot, enabling single-cycle dual-side processing, boosting output 40% and freeing operators.

Solution By
OptiPro
OptiPro
Published
February 17, 2026
Last Updated July 16, 2026
Share Facebook X LinkedIn Email Copied link
OptiPro Video courtesy of OptiPro
White collaborative robot arm with a black tool attachment positioned over a small metal fixture inside a factory work cell with clear plastic safety panels, other machines visible in the background.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/cobot-beveling-and-fanuc-machining-centers-boost-quality-and-productivity-for-optics-manufacturer

Challenges

01

Tedious, manual bevel process

02

Ergonomic challenges for staff

03

Ramping up production

04

Inconsistent quality

Results

Young generation 4

Frees up employees

Optimization 7

40% increase in production

Quality improvement 2

Eliminates ergonomic concerns

Proven technology 8

Consistent results achieved

White collaborative robot arm with a black tool attachment positioned over a small metal fixture inside a factory work cell with clear plastic safety panels, other machines visible in the background.

Story

Sydor Optics, a global leader in custom optical manufacturing based in Rochester, NY, produces high precision optics using advanced fabrication technologies. The company sought to optimize its manual beveling process, which was tedious, labor intensive, and ergonomically challenging.

To automate the process, Sydor purchased an OptiPro Revel, a turnkey robotic beveling solution. This FANUC Cobot and Go system employs a FANUC CRX-10iA/L collaborative robot, enabling each part to be beveled on both sides in one uninterrupted cycle.

This automated solution has increased Sydor’s daily production throughput by approximately 40 percent. The Revel can run unattended, freeing employees for other tasks and increasing beveling time during off shifts. Additionally, the system produces parts with consistent quality, reducing variability and rework.

With this automation, as well as the company’s CNC machining success using FANUC ROBODRILL Plus machining centers, Sydor Optics delivers high quality parts on time and to specification—allowing them to meet and exceed customer expectations.

F04 A0005
"

When we were doing it manually, it would take—for one tray of parts—eight and a half to nine hours for someone to do it. Now with the Revel, it takes five hours, which is almost a 40% increase of productivity, and that operator is now freed up to run other machines.

Joe DiFrancesco CNC Manager – Sydor Optics

FANUC Products Used

White FANUC CRX CRX-10iA/L-series collaborative robotic arm with green accents on a black base.
Collaborative

CRX-10iA/L

Boost productivity with the user-friendly FANUC CRX-10iA/L cobot featuring a 10kg payload, 1418mm reach, and simple programming.

Max Payload:
10 kg
Reach:
1418 mm
View CRX-10iA/L
A D21 Mi B5 PLUS L 01 4 C
ROBODRILL

α D21MiB5 Plus

Standard-stroke ROBODRILL delivering high-precision, flexible milling and drilling with adaptable options for high-productivity machining.

View α D21MiB5 Plus
FANUC ROBODRILL a D21MiB5ADV Plus
ROBODRILL

α-D21MiB5 ADV Plus

Standard-stroke ROBODRILL delivering high-capacity, high-precision milling and drilling with adaptable performance and a 400 kg table load.

View α-D21MiB5 ADV Plus
OptiPro
FANUC Authorized System Integrator

OptiPro

As a FANUC America Authorized Systems Integrator (ASI), OptiPro is dedicated to providing robotic automation solutions that help manufacturing companies achieve more efficient production. Our Automation team consists of trained technicians as well as mechanical, electrical, and software engineers that you can rely on throughout the entire collaboration process.

Visit Website https://www.optipro.com/automation-solutions
Sydor optics logo
End User

Sydor Optics

Not only does Sydor Optics offer the best in double-sided grinding and polishing services, we offer the largest number of polishing machines in the US to cover your plano optics needs — from the smallest to largest available.

Visit Website