Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. How Zenni Optical Built a Faster, Smarter, More Scalable Fulfillment Line

How Zenni Optical Built a Faster, Smarter, More Scalable Fulfillment Line

Zenni Optical scaled fulfillment by partnering with OSARO to automate robotic bagging with FANUC robots, boosting speed, accuracy, and growth readiness.

Solution By
OSARO LOGO RGB GRADIENT 2
OSARO
Published
February 9, 2026
Last Updated August 13, 2026
Share Facebook X LinkedIn Email Copied link
OSARO Video courtesy of OSARO
M 10i D 12 Handling Packages
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/how-zenni-optical-built-a-faster-smarter-more-scalable-fulfillment-line

Challenges

01

Increasing fulfillment volume driven by rapid growth

02

Manual packaging steps limiting throughput

03

Need for consistent, high accuracy barcode scanning through opaque cases

04

Desire to reduce manual touchpoints without compromising quality

Results

Trending up 4

Reduction of manual handling steps from five to two

Optimization 8

80% increase in throughput

Quality improvement 2

Reliable end to end automation

Proven technology 8

Near zero scanning errors thanks to integrated vision and ML

M 10i D 12 Handling Packages

Story

California-based eyewear brand Zenni Optical has built its reputation on delivering affordable, high quality eye glasses to millions of customers worldwide. With annual sales of six to seven million pairs—and double digit growth every year—the company’s distribution and fulfillment operations must run with precision and speed.

“Anyone wearing eyeglasses is our customer,” said Simon Goh, Director of Distribution and Facilities at Zenni Optical, who explained that as volume increased, so did the critical need to scale smartly.

Zenni had explored robotics for years, but earlier solutions lacked the flexibility and intelligence required for their unique packaging workflow. The challenge centered on reliably scanning barcodes through Zenni’s branded eyeglass cases—something traditional systems struggled to do consistently at high speed.

That changed when Zenni discovered OSARO.

“When it comes to machine learning, AI, and vision, OSARO actually has an all in one solution,” Goh explained. OSARO specializes in warehouse automation, focusing on applications like kitting, depalletization, and robotic bagging. For Zenni, OSARO deployed a robotic bagging cell powered by FANUC industrial robots and OSARO’s machine learning driven perception software.

The robotic cells pick up each pair of eyeglasses in its protective case, scan the unique barcode through the case, and place the item into an automated bagging machine. The system then seals the package and sends it directly into the shipping stream.

To achieve the required scanning accuracy, OSARO integrated Cognex vision technology alongside FANUC robotics and industrial automation components from long time partners FANUC and PreciTaste. The combination delivered the reliability Zenni needed.

“The scanning part is crucial,” Go noted. “Once OSARO brought in the Cognex scanner, scanning became the least of our concerns.” Before automation, the packaging workflow required five manual steps. With the robotic system in place, Zenni reduced manual steps to just two.

“We always try to get to 100% accuracy, which is very difficult,” Go said. “But the robot’s design and process reduce errors to nearly zero.”

OSARO’s HyperCare™ customer success model ensured Zenni had hands on support throughout installation, commissioning and ongoing operation. “We have to integrate with so many different pieces of equipment,” Go said. “It would be impossible without a professional company like OSARO.”

Since deployment, Zenni has seen an 80% increase in throughput, along with more consistent quality and a more scalable fulfillment process. With automation proving its value, Zenni is well positioned to continue expanding its product offerings and customer base.

Simon goh
"

Our customers and potential customers can see we’re committed to the future. Our willingness to commit to automation makes a statement that says we’re going to be around a long time.

Simon Goh Director of Distribution and Facilities – Zenni Optical

FANUC Products Used

M-10iD/12
Articulated Robots

M-10iD/12

The FANUC M‑10iD/12 is a compact 6 axis robot that reaches the highest axis speed and precision in its class.

Max Payload:
12 kg
Reach:
1441 mm
View M-10iD/12
OSARO LOGO RGB GRADIENT 2
FANUC Authorized System Integrator

OSARO

OSARO is a leading provider of AI-powered robotics solutions for e-commerce, logistics, and manufacturing. The company’s machine-learning software enables industrial robots to perceive, grasp, and manipulate a wide variety of objects, streamlining complex tasks like piece-picking, kitting, and bagging. OSARO’s intelligent automation solutions improve efficiency, reduce costs, and drive productivity across global fulfillment networks.

Visit Website https://www.osaro.com
Zenni Optical Logo
End User

Zenni Optical

Zenni pioneered the online eyewear industry in 2003 with a mission to make eyewear affordable and accessible to everyone. With complete prescription pairs starting at under $10, Zenni offers adults and children the freedom to see clearly and express themselves through a large collection of high-quality prescription glasses, sunglasses, protective eyewear and non-prescription glasses, all curated with a sense of fashion and dynamic style. Based in the San Francisco Bay Area, the company has brought massive price disruption to the traditional retail model. With over 51 million frames sold worldwide, Zenni is proud to be the Official Eyewear of the San Francisco 49ers, Boston Celtics, Chicago Bulls, Monster Jam, Ghost Gaming and more. Zenni has worked with designers and tastemakers on curations and collections, including Chase Stokes, Sam Cassell and George and Claire Kittle.

Visit Website