Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Painting in Partnership: Regal Finishing Elevates Its Paint Operations with RTSS’ Automation Solution

Painting in Partnership: Regal Finishing Elevates Its Paint Operations with RTSS’ Automation Solution

Regal Finishing partnered with RTSS and FANUC to automate painting, consolidating complex processes into a single system for consistency and efficiency.

Solution By
Robotic Technical Support Services, Inc. (RTSS)
Robotic Technical Support Services, Inc. (RTSS)
Published
January 22, 2026
Last Updated October 15, 2026
Share Facebook X LinkedIn Email Copied link
Robotic Technical Support Services, Inc. (RTSS) Video courtesy of Robotic Technical Support Services, Inc. (RTSS)
FANUC P-50iB paint robot spraying coating onto curved parts hanging on a rack inside a paint booth
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/painting-in-partnership-regal-finishing-elevates-its-paint-operations-with-rtss-automation-solution

Challenges

01

Multiple stage paint process

02

Excessive part handling

03

High scrap and rework levels

04

Skilled labor hurdles

05

Throughput limitations

Results

Trending up 4

Improved overall daily throughput by about 125%

Optimization 8

Reduced scrap and rework, part handling and process complexity

Quality improvement 2

Increased first run good parts by about 35%

Proven technology 8

Consolidated paint process into a single, four-stage automated line

Young generation 4

Redeployed skilled painters, requiring only for specialized customer requests

Maintenance health 2

Established a consistent, repeatable coating process to support new customer acquisition and future growth

FANUC P-50iB paint robot spraying coating onto curved parts hanging on a rack inside a paint booth

Story

For decades, Regal Finishing has earned a reputation for delivering high quality coatings in applications where consistency and performance are critical. As product complexity increased and quality expectations rose, Regal’s traditional painting operations became increasingly difficult to manage. Multiple paint lines, excessive part handling, and rising scrap levels needed to be resolved so the company’s growth could continue.

To overcome these challenges, Regal Finishing partnered with Robotic Technical Support Services (RTSS) and FANUC America to design and implement a fully automated robotic paint line. The objective was straightforward: consolidate painting into a single, end-to-end process that would improve consistency, reduce waste, and increase throughput while maintaining the level of quality customers expect.

The new system, integrated by RTSS, features FANUC P-50iB paint robots arranged in a multi-zone, conveyor-fed layout. This configuration allows Regal to apply multiple coatings — primer, base, specialty finishes and clear coat — in one pass. By consolidating operations into a single line, Regal dramatically reduced part handling while improving first pass quality and overall efficiency. Just as important, the modernized facility reflects Regal’s long term commitment to advanced manufacturing and continuous improvement.

Since implementing the automated paint line, the company has seen significant measurable improvements across its operation. Previously, the process required six painters across four manual paint booths and two older automated lines.

A review of two part numbers being produced by Regal and show the benefits of the collaboration with RTSS.

Part #1:

  • Prior to the new robotic paint line about 150-175 pieces were produced per shift.
  • After integration of the new automation system, production ramped up to about 300-350 pieces per shift.
  • That’s a 133% increase throughput and approximately a 35% improvement in first run good parts.

Part #2:

  • Prior to the new robotic paint line, production totaled about 300-400 sellable pieces per shift.
  • After integration of the new automation system, production is about 600 – 700 sellable pieces per shift.
  • That’s approximately a 75% increased throughput and about a 35% increase in first run good parts.

Labor and Material Savings, and Line Utilization:

  • Produced 50% salary savings, down from six painters to only three operators required.
  • Paint material usage has seen about 10-15% cost savings.
  • Including increased throughput, and the line has availability for about 33% more utilization.

Not only does the data show greater output and lower costs, but it also means increased profits and greater confidence in meeting customer demand.

Jim Kodis Quote
"

Our customers and potential customers can see we’re committed to the future. Our willingness to commit to automation makes a statement that says we’re going to be around a long time.

Jim Kodis President – Regal Finishing

FANUC Products Used

P 50ib 10l updated beauty shot
Paint

P-50iB/10L

The FANUC P‑50iB/10L is an ultra compact, high reach robot that provides a reliable and precise painting and coating solution for a huge range of industries.

Max Payload:
10 kg
Reach:
1800 mm
View P-50iB/10L
Robotic Technical Support Services, Inc. (RTSS)
FANUC Authorized System Integrator

Robotic Technical Support Services, Inc. (RTSS)

RTSS has been providing solutions since 2012. RTSS designs and delivers turnkey industrial robotic systems for factories and manufacturers. Programming and preventive maintenance services are additional key services RTSS provides to keep its customers making parts and profits. One primary specialty of RTSS is robotic paint, spray and dispense applications. RTSS also delivers robust automation solutions for machine tending, material handling, and palletizing. RTSS understands the intricacies of engineering automation processes and works closely with its customers to deliver exceptional solutions that exceed their expectations.

Visit Website https://www.robotictss.com
Regal finishing logo
End User

Regal Finishing

Regal Finishing is located in Coloma, Michigan. The company provides customer finishing solutions to customers in the aerospace, appliance, automotive, cosmetics, communications, hardware, electric, lighting, medical and transportation industries. Regal Finishing vacuum metallizes, EMI/RFI shields, paints, pad prints, and sub‑assembles for production and development projects. In addition to finishing customer supplied parts, Regal Finishing also partners with injection molders, blow molders, extruders, metal formers and casters to offer a complete product.

Visit Website