See how Gateway Technical College in Southeast Wisconsin uses FANUC products to give students the real-world skills they need to power the future of manufacturing!
FANUC has more than 1,400 partner schools that offer our education and certification programs using the latest automation technologies. Students at partner schools are prepared to enter the workforce with the skills and knowledge aligned to today’s industry technology. Talk to us today to learn how we can help.
Contact us
The FANUC LR Mate Robot Series of human arm-sized robots are your best compact solution for fast handling and processing parts up to 14 kg across a whole range of industries.
These small payload tabletop robots can be equipped with an array of intelligence features including robot vision & Force sensing functionality for even higher levels of accuracy and productivity.
Learn More
The new-generation ROBODRILL promises unrivaled quality and precision at great hourly rates. At the heart of every ROBODRILL is a patented high-speed tool changer that can carry 21 tools and offers the best reliability in its class. This makes it extremely resistant to radial forces and enables it to deliver unbelievably efficient machining.
With an unbeatable tool change time of 0.7 seconds and a turret capable of handling tools weighing 4 kg, the new advanced version is both the fastest and strongest vertical machining center on the market.
There is a growing need for skilled workers competent in the setup, programming and operation of CNCs.
FANUC America provides CNC Simulators for both manufacturers looking to train in-house using real FANUC equipment, but without taking a machine out of production.
FANUC brings together robotics and automation with advanced analytics to drive smarter, faster business decisions for industrial companies.
We're here to help prepare students for exciting careers in automation! Fill out the form below and a knowledgeable FANUC Certified Education Sales Representative will be in touch.