For nearly two decades, Trantech Radiator Products in Edgefield, South
Carolina, has been running FANUC robots for 2-3 shifts a day for 6-7 days a
week. As the largest transformer radiator manufacturer in North America, they
once again turned to automation—this time to modernize a complicated and
outdated brazing process that was hindering their business’s ability to remain
competitive.
After vetting several potential automation partners, Trantech turned to FANUC
Authorized System Integrator WeldBot to design and deliver a solution that
would allow them to achieve increased throughput and repeatability while still
allowing for necessary, slight inconsistencies in parts.
Using MIG wire, the FANUC ARC Mate robot welds radiator joints together
creating a stronger bond between the two pieces of metal than existed with the
previously used brazing method.
Equipped with a Servo Robot laser, the WeldBot system accommodates bow and
deflection that results from resistance welding while reducing repairs a
significant 50-80 percent. Without as much rework, three upstream processes
were eliminated. This is all in addition to an increased throughput of
approximately 30 percent, which allows the company to keep up with increasing
market demand.
Today, Trantech has two WeldBot systems in place, and has modernized operations, realized
significant operational savings and strengthened the quality of their
products.
“It’s a great advantage for us to have this,” says John Mathis, Trantech
material manager,” and I’m looking forward to it helping the plant continue to
grow.”