Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Automating Agriculture: Greenhouse Turns to Robots for Tomato Harvesting

Automating Agriculture: Greenhouse Turns to Robots for Tomato Harvesting

To offset rising labor costs, Westburg Greenhouse adopted Four Growers’ FANUC-powered GR-200 robot to automate tomato harvesting and boost sustainability.

Solution By
Four growers logo
Four Growers
Published
October 27, 2025
Last Updated September 21, 2026
Share Facebook X LinkedIn Email Copied link
Four Growers Video courtesy of Four Growers
Close-up of a black robotic arm end effector positioned among tomato vines with ripening red, orange, and green cherry tomatoes in a greenhouse setting.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/automating-agriculture-greenhouse-turns-to-robots-for-tomato-harvesting

Challenges

01

Rising labor costs

02

Speed and accuracy of harvesting

Results

Trending up 4

Rapid deployment — robots operational within one week

Proven technology 8

Elevated productivity – around the clock harvesting

Young generation 4

Significant harvest labor savings achieved through automated harvesting so that the labor force could focus on other tasks

Delivery

Delivered one of the first commercially scaled, automated harvesting fleets

Career

Future scalability, with plans to adapt the same platform for cucumbers and peppers

Close-up of a black robotic arm end effector positioned among tomato vines with ripening red, orange, and green cherry tomatoes in a greenhouse setting.

Story

Labor costs for greenhouse operators have been increasing for many years. To get labor costs under control and become future proof automation is needed. Westburg Greenhouse, a commercial grower located in the Netherlands, sought a scalable solution to automate harvesting while maintaining quality and efficiency.

Four Growers, a category leader in intelligent ag-tech platforms, developed the GR-200 robotic harvesting platform, powered by FANUC’s LR Mate robot. The system combines AI-driven vision and motion planning to identify and harvest ripe tomatoes with quick precision. FANUC’s robot was selected for its speed, payload capacity, reach, compact footprint and ease of use — all critical factors for greenhouse environments.

Westburg Greenhouse partnered with Four Growers to deploy the first operational fleet of GR-200 LR Mate robots. Within a week of installation, the robots were harvesting tomatoes, significantly reducing the need for manual harvesting labor.

The robots now harvest grape and cherry tomatoes around the clock, resulting in fewer people being needed for the harvesting process and freeing staff to focus on other crop tasks. With custom AI models and datasets, the system adapts to each grower’s ripeness standards and crop types. Westburg plans to expand its fleet and automate additional activities.

This milestone marks a major step toward future-proofing greenhouse operations — enabling growers to produce high-quality, sustainable food efficiently and affordably.

Bas van Leeuwen
"

Thanks to the robot fleet day-and-night harvesting, we can complete the harvesting process with fewer people. This allows us to perform the crop work at the next level and elevate our entire business operations. We are looking forward to scaling up with Four Growers and work with more robots.

Bas van Leeuwen CEO – Westburg

FANUC Products Used

LR Mate 200iD/7L
Articulated Robots

LR Mate 200iD/7L

Fast at handling small payloads, the FANUC LR Mate 200iD/7L compact multi-purpose industrial robot offers an enhanced reach at 911mm and payloads of up to 7 kg.

Max Payload:
7 kg
Reach:
911 mm
View LR Mate 200iD/7L
Four growers logo
FANUC Authorized System Integrator

Four Growers

Four Growers, a FANUC Authorized System Integrator, was founded to provide healthy, affordable, local produce by reducing the production costs of greenhouse growers through robotic technology. Our technology currently optimizes autonomous tomato harvesting and will soon be available for pepper and cucumber crops.

Visit Website https://fourgrowers.com/
Logo WB snack tomato specialist
End User

Westburg, Snack Tomato Specialist

Westburg is specialized in the cultivation and processing of the top segment snack tomatoes. Westburg grows red, yellow, orange, brown and ivory-colored snack tomatoes on 14 hectares in 3 greenhouses in Grubbenvorst (Limburg, the Netherlands). Westburg grows with its customers as the year-round color specialist in Northern Europe in snack tomatoes. Growing through cooperation and intensification with chain partners. Brothers Bas and Ton van Leeuwen are the proud entrepreneurs of Westburg.

Visit Website