Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Steelway Boosts Beam Welding Productivity with New Robotic Integration

Steelway Boosts Beam Welding Productivity with New Robotic Integration

Steelway automated beam welding with AGT Robotics, using dual FANUC Arc Mate robots to boost capacity, streamline long-beam welds, and redeploy welders.

Solution By
AGT Robotics
AGT Robotics
Published
November 13, 2025
Last Updated September 11, 2026
Share Facebook X LinkedIn Email Copied link
AGT Robotics Video courtesy of AGT Robotics
A yellow AGT Robotics welding arm performing arc welding on a large rectangular metal beam mounted on a rotating fixture, inside an orange-fenced industrial work cell.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/steelway-boosts-beam-welding-productivity-with-new-robotic-integration

Challenges

01

Difficulty finding labor

02

Limited production capacity

03

Inefficient automation system

Results

Optimization 8

Faster throughput

Footprint

Expanded and optimized workspace

Young generation 4

Associates moved into higher quality roles

A yellow AGT Robotics welding arm performing arc welding on a large rectangular metal beam mounted on a rotating fixture, inside an orange-fenced industrial work cell.

Story

Steelway Building Systems, a leading manufacturer of steel structures based in Elmer, Ontario, faced a familiar challenge in today’s industrial landscape: a shortage of skilled welding labor. Located in a rural area, the company struggled to attract and retain qualified welders, which began to impact throughput and operational efficiency. With a commitment to continuous improvement and product excellence, Steelway’s leadership sought a solution that could not only fill the labor gap but also elevate productivity across its beam welding operations.

Last year at the Fabtech tradeshow in Chicago, Steelway discovered AGT’s advanced robotic welding system, BeamMaster, a game-changing solution capable of rotating beams for full four-sided weld coverage. Impressed by the system’s capabilities, Steelway partnered with the FANUC Authorized System Integrator to bring the technology to their facility.

The goal: automate the welding of three-plate beams to increase output, reduce manual workload and optimize efficiency.

The results were immediate and measurable. The new system allowed Steelway to weld all four sides of a beam without manual repositioning, significantly speeding up production. Welders were redeployed to focus on finishing tasks, while the robot handled the bulk of repetitive welding.

“It’s better, easier to learn, and capable of more welding than our previous system,” said Randy Thiesen, a Steelway robotic weld cell coordinator.

Encouraged by the success of the new BeamMaster system, Steelway expanded by adding a second robot and extending the weld zone by 15 feet, which accommodates beams up to 60 feet long. This dual-zone setup enabled simultaneous welding of long and short beams, maximizing throughput and floor space utilization. The integration with Advanced Steel and Cortex software allowed seamless programming via IFC file exports, streamlining the transition from design to production.

Steelway’s investment in automation has not only addressed labor shortages but also positioned the company for scalable growth. With plans to extend robotic welding into its hot-rolled structural section, Steelway continues to push the boundaries of what’s possible in steel fabrication.

Jake Giesbrecht
"

The future for us is to buy more robots, and we’d like to continue to add on to the ones we have today.

Jake Giesbrecht Director of Product Excellence – Steelway Building Systems

FANUC Products Used

Yellow FANUC ARC Mate 120iD/12L robotic welding arm with a Lincoln Electric AUTODRIVE wire feeder and black welding torch, shown against a white background with its arm extended horizontally to the right.
Arc Welding

ARC Mate 120iD/12L

Long-arm model of the ARC Mate 100iD series featuring outstanding axes speed and ultimate precision with extra reach.

Max Payload:
12 kg
Reach:
2272 mm
View ARC Mate 120iD/12L
AGT Robotics
FANUC Authorized System Integrator

AGT Robotics

Based in Trois-Rivières, Québec, AGT Robotics is the global leader in robotic welding solutions for the structural steel industry. Through intelligent automation and its proprietary Cortex software, AGT enables fabricators to weld faster, smarter, and with less dependence on skilled labor.

Visit Website https://agtrobotics.com/
Steelway logo
End User

Steelway Building Systems

Founded in 1976, Steelway is a family-owned and operated manufacturer of customized steel building solutions. A life-long passion for design and building along with an entrepreneurial spirit that has been passed down from a father to his sons is what defines our company culture. Honouring that legacy, our primary focus is fostering and maintaining positive long-term relationships with our clients, employees, and suppliers as well as the community in which we work and live.