FANUC America, a global industrial automation leader, will demonstrate its unmatched food-grade robotic and automation solutions at PACK EXPO Las Vegas, Sept. 29-Oct. 1, at the Las Vegas Convention Center in booth W-3408.
For Immediate Release
ROCHESTER HILLS, MI – (September 22, 2025) –
FANUC America, a global industrial automation leader, will demonstrate its
unmatched food-grade robotic and automation solutions at PACK EXPO Las Vegas,
Sept. 29-Oct. 1, at the Las Vegas Convention Center in
booth W-3408.
Each PACK EXPO demonstration highlights FANUC’s commitment to sanitation and
safety without compromising performance, featuring products equipped with
NSF-H1 certified food-grade grease for internal mechanical components,
IP69K-rated protection against water and dust ingress, hygienic
washdown-capable designs for cleaning and sanitation procedures, and advanced
vision-guided automation that enables robots to detect, track and respond to
variable product positions. From food-grade cobots handling chocolate chip
cookies and palletizing boxes to robots slicing brownies and packing sausages,
FANUC’s diverse lineup of technologies is designed to automate both primary
and secondary food-handling tasks.
These innovations help food manufacturers address labor shortages, improve
sanitation and increase throughput while maintaining consistent quality.
Picking, Packing and Palletizing Innovation in Action
CRX Food-Grade Cobots – Hygienic, Flexible and Easy to Deploy
- Dual CRX-20iA/L Baking Chocolate Chip Cookies
A
CRX-20iA/L
mounted with 3DV/400 vision loads chocolate chip cookies onto a conveyor
belt where the sweet treats pass through a simulated oven. A second
CRX-20iA/L equipped with a robot mounted 3DV/200 then uses conveyor
tracking to catch the baked cookies as they come off the conveyor belt,
place them on a tray before putting the full tray onto a cart that has been
located using FANUC iRVision One Marker Offset. Designed for food
environments, the cobots use NSF-H1 food-safe grease for component
lubrication, white epoxy coating for visibility and cleanliness, and are
IP67 rated to ensure hygienic handling and reduce manual labor in bakery
operations.
- CRX-30iA Palletizing Packaged Food Boxes
FANUC’s largest food-grade cobot builds two pallet stacks using
PalletTool 3, a powerful software solution designed to simplify and
accelerate robotic palletizing setup and operation. A Multi-Case Gripper
end-of-arm tool is applied to dramatically increase throughput. The
CRX-30iA
uses NSF-H1 food-safe grease for component lubrication, white epoxy coating
for visibility and cleanliness and is IP67 rated to ensure hygienic handling
and reduce manual labor in bakery operations. Ideal for secondary packaging,
the system supports safe and scalable palletizing in food production.
LR Mate Robots – Compact, Washdown-Capable and Versatile
- LR Mate/10-11A Food/Clean Packing Frozen Protein Bags
In this all-new cell, a washdown-capable
LR Mate robot with stainless
steel wrist flanges and NSF-H1 grease picks bags of frozen meatballs from a
moving conveyor and places them into a case. The system uses an
iRVision 3DV/400 camera and iRPickTool – an advanced line
tracking software that enables FANUC robots to perform high-speed
pick-and-place operations, making it ideal for cold chain and frozen food
packaging.
- Dual R-50iA LR Mates Picking and Palletizing
A unique demonstration highlights the advanced capabilities of
FANUC’s new R-50iA controller, featuring two FANUC LR Mate industrial robots performing bin picking
and palletizing.
The compact LR Mate/7-7D robot with FANUC’s 3DV/400 vision camera bin
picks jumbled boxes from a container onto a conveyor. This robot is running
python code natively on its paired FANUC controller. The second robot, an LR
Mate/7-9D long arm unit with a 3DV/400 camera and PalletTool 3, identifies
the size of the box on the conveyor and palletizes it onto the appropriate
pallet. This controller showcases new cybersecurity protocols including MQTT
TLS, the use of a LDAPS server for user access control along with Software
PLC capability for cell control and HMI functionality. Additionally, our new
Teach Pendant with lighter weight and enhanced performance is featured.
High-Speed Food Handling – Delta and SCARA Robots for Primary Packaging
- DR-3iB/6 Stainless and SR-12iA/C Packing Sausage
Products
This demo shows the
DR-3iB/6 Stainless
IP69K-rated delta robot and a food-grade
SR-12iA/C
SCARA robot placing sausage links in packages. Driven by USDA and FDA
sanitation standards, the system uses vacuum grippers and FANUC’s
iRPickTool for accurate placement in high-pressure washdown
environments.
- SR-12iA/C Cutting Brownies
In this all-new
cell, a food-grade SCARA robot
guided by iRVision 3DV/400 cameras, is equipped with a dynamic end
effector to pick brownies from a conveyor and place them into cutting
fixtures. An ultrasonic knife performs clean and consistent cuts on the
brownies. Designed for ready-to-eat bakery environments, it meets sanitation
needs for high-precision dessert handling.
End-of-Line and Secondary Packaging – Palletizing and Software Solutions
- M-710/50-26D Palletizes and Depalletizes Crates of Tortillas
In this all-new demo, FANUC’s
M-710/50-26D Food
Option robot with food-grade grease demonstrates a robust palletizing and
depalletizing system using FANUC’s PalletTool 3 and Dual Check Safety
software packages. The robot picks and places a pallet from a dispenser,
then picks crates of packaged tortillas from two conveyors and stacks them
onto the pallet. Once the pallet is full, the robot reverses the process,
returning the crates to the conveyors and the pallet to its dispenser.
Combined with Dual Check Safety software, the robots curved J2 arm allows it
to work close to obstacles in the cell, creating an exceptionally compact
end-of-line palletizing solution without compromising robot speed, reach or
payload. This solution highlights FANUC’s ability to automate repetitive
tasks for the safe handling of packaged foods in distribution environments.
- M-410/800F-32C Static Layer Palletizing Display
In
this all-new static display, FANUC’s
heavy-duty M-410/800F-32C robot
with a modular layer gripper showcases its capability to handle large
payloads in high-volume operations. With an 800 kg payload capacity, no job
in food logistics is too big for the M-410/800F-32C.
- PalletTool 3 Kiosk – Software for Food PalletizingExplore
FANUC’s latest palletizing software through a hands-on kiosk. Using
ROBOGUIDE
simulation and a
Tablet Teach Pendant, users can create unit loads and test features like the Custom Pattern
Editor software and Multi-Case Gripper end-of-arm-tool. With quick and easy
setup combined with unmatched capability and scalability, PalletTool 3
streamlines palletizing in food and beverage environments.
“FANUC continues to lead the industry in developing food-grade cobot and robot
solutions that meet the highest standards for hygiene, reliability and
performance,” said Eric Potter, General Manager, Robot Application
Engineering, FANUC America. “Our technologies help food manufacturers automate
safely and efficiently to overcome labor challenges, boost productivity and
maintain consistent quality in demanding environments.”
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and
provides industry-leading CNC systems, robotics and ROBOMACHINEs.
FANUC’s innovative technologies and proven expertise help manufacturers
in the Americas maximize productivity, reliability and profitability.
Headquartered in Rochester Hills, Mich., FANUC America has facilities
throughout North and South America. Visit
www.fanucamerica.com
for more information or explore the CRX line of cobots at
CRX.FANUCAmerica.com.
Connect with FANUC America on
YouTube, X,
Facebook,
LinkedIn
and
Instagram.
FANUC America Corporation PR Contact:
[email protected]