Have questions for FANUC Mexico?

FANUC Mexico offers its experienced team to help solve the most complex automation challenges for any size business.

Contact Us 

iRVision-2D Operation and Programming

Course Code: iRvision-2D-R30iA
2 DAYS / 16 HOURS

This course covers the basic areas and procedures required for an operator, technician, or programmer to configure, teach, test, and modify iRVision applications on R-30iA controllers.

Objetivos del Curso:

  • Turn on and move the robot
  • Set up communication between the robot and the teaching computer
  • Configure and calibrate the camera
  • Teach a vision process (stationary camera)
  • Teach a vision process (camera mounted on the robot)
  • TPP Programming
  • Common faults and alarms

Audience

This course is designed for people who need to install, configure, program, or troubleshoot a FANUC iR-Vision system.

Prerequisites

Programming and Operation of Software Handling Tool, Spot Tool, Arc Tool or Dispense Tool.

Complete Description

The course consists of theoretical exposition in the classroom, demonstrations, practical exercises, designed to reinforce learning.

Exam Note

In order to identify the level of initial knowledge and achievement during the course, an exam is applied at the beginning of the course and another at the end.

Security Note

All exercises performed during the course include recommended safety procedures.

Teaching Materials

La documentación y material didáctico se entrega en idioma inglés.