Contents
As manufacturing continues its shift toward digital-first engineering, simulation and virtual commissioning are becoming essential tools for reducing risk, accelerating timelines and improving overall system performance. Reflecting growing demand for easier integration, FANUC America has released enhancements to its ROBOGUIDE® simulation software that simplify connectivity with Rockwell Automation’s FactoryTalk® Logix Echo.
The update, introduced as part of ROBOGUIDE Version 10 (revision E), simplifies how manufacturers design, test and validate automation systems—all before a single piece of physical equipment is installed.
Simplifying Virtual Commissioning Workflows
At the heart of this update is improved integration between FANUC’s virtual robot controllers and Rockwell’s virtual PLC environment via Logix Echo. These enhancements, including support for Logix Echo’s handshake protocol, help manufacturers accelerate testing, enhance system validation and reduce costs.
Previously, configuring communication between virtual robots and PLCs required multiple manual steps. FANUC’s latest update eliminates much of that complexity. A new user-friendly interface automatically assigns unique IPv4 aliases and simplifies network configuration, making it easier to expose virtual controllers to external networks and enable EtherNet/IP communications.
Support for Logix Echo’s handshake protocol further enhances synchronization between systems, enabling more accurate testing scenarios and robust system validation.
The result is a more streamlined workflow that reduces setup time and allows engineers to focus on refining application performance rather than troubleshooting connectivity.
Driving Efficiency and Reducing Risk
Virtual commissioning continues to gain traction across manufacturing sectors, particularly as companies seek to minimize downtime and avoid costly rework during system startup. By debugging and validating systems in a virtual environment, manufacturers can identify and resolve issues early in the design phase.
This capability is especially valuable for complex or first-of-its-kind automation cells, where physical testing can be time-consuming and expensive. With ROBOGUIDE and Logix Echo working together, engineers can simulate full system behavior—including robot motion, PLC logic and network communication—before deployment.
Extending Value Across Industries
Within FANUC, virtual commissioning has already demonstrated measurable impact—particularly in its Paint and Sealing business. Engineers are able to evaluate electrical systems, verify wiring schemes, and validate robot paths digitally, identifying potential issues long before installation begins.
For system integrators, the benefits extend beyond internal efficiencies. Virtual environments allow them to collaborate with customers earlier in the project lifecycle, offering proactive support and resolving issues remotely. This approach not only accelerates project timelines but also reduces disruptions once systems are live.
In some cases, integrators can even diagnose and correct system malfunctions in a virtual model while production continues uninterrupted—an advantage that underscores the growing importance of digital tools in modern manufacturing.
Built-In Integration, Immediate Access
The connection between ROBOGUIDE and FactoryTalk Logix Echo is built directly into the latest software release, eliminating the need for additional middleware or custom development. Users simply need the appropriate licenses for both platforms to take advantage of the integration.
This out-of-the-box compatibility reflects FANUC’s commitment to making advanced simulation tools more accessible and practical for everyday engineering use.
Supporting the Future of Digital Manufacturing
The adoption of virtual commissioning is expected to continue rising as manufacturers prioritize shorter startup times, improved software quality and enhanced safety. As production environments become more complex, the ability to test and validate systems virtually will play an increasingly critical role in maintaining competitiveness.
FANUC’s latest ROBOGUIDE enhancements position the company—and its customers—to take full advantage of this shift, delivering smarter, faster and more reliable automation solutions.
Learn More: Manufacturers, integrators and students interested in exploring FANUC’s simulation tools can access additional resources through the company’s Tech Transfer website. The site offers engineer-led tutorials, programming tips and practical guidance for working with FANUC robots and cobots.
Free registration is required to access Tech Transfer content.