Skip to content Skip to navigation
Resources About MyPortal Login
Edit Entry
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
Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Automation Helps Seibel Modern Successfully Tackle Large Welding Project

Automation Helps Seibel Modern Successfully Tackle Large Welding Project

Seibel Modern cut welding touch-up 50% and streamlined production using a FANUC CRX cobot, delivering miles of bridge fencing efficiently.

Solution By
Properlyworks logo
Properly Works
Published
May 23, 2024
Last Updated October 22, 2026
Share Facebook X LinkedIn Email Copied link
Properly Works Video courtesy of Properly Works
A white FANUC collaborative robot arm with green accent rings welding steel beams in a work cell, with blue welding light glowing at the torch and a red curtain behind it.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/automation-helps-seibel-modern-successfully-tackle-large-welding-project

Challenges

01

Automate a large project to weld miles of fencing

02

Increase welding speed and consistency

03

Reduce the amount of weld touch-ups

Results

Proven technology 5

Flagging system keeps production on schedule.

Product range 1

Higher quality welds - touch-up work has been reduced by 50%.

Young generation 4

CRX Cobot is easy to learn and use.

A white FANUC collaborative robot arm with green accent rings welding steel beams in a work cell, with blue welding light glowing at the torch and a red curtain behind it.

Story

Seibel Modern, based in Lancaster, NY has been a leading supplier of industrial and custom welding services for over 75 years.

A major contract to weld fencing for a large bridge project prompted Seibel Modern to select FANUC’s Authorized System Integrator Properly Works to provide an automation solution to help them weld over three miles of fencing.

Initially various processes worked independently, which fell short of efficiency goals. Properly Works brought all the various operations together into a safe and streamlined operation. System implementation was seamless, and Seibel Modern’s employees quickly learned how to operate the CRX-10iA/L welding cobot and other equipment.

Property Works also integrated a graphically illustrated flagging system which was instrumental in keeping production on schedule. The flagging system shows an image of the actual fence and highlights each completed weld. If there are any issues related to a weld such as a non-start or the welding wire getting stuck, the operator can simply unflag the weld, and the robot will return to that location and redo that weld.

A key benefit of the automated solution is that touch-up work has been reduced by 50%, which is a huge time saver. In addition, Properly Works personnel have gone above and beyond in terms of customer support and Seibel Modern plans to continue the relationship on future automation projects.

Brandon kujawa
"

A key benefit of the automated solution is that touch-up work has been reduced by 50%.

Brandon Kujawa Seibel Modern

FANUC Products Used

White FANUC CRX CRX-10iA/L-series collaborative robotic arm with green accents on a black base.
Collaborative

CRX-10iA/L

Boost productivity with the user-friendly FANUC CRX-10iA/L cobot featuring a 10kg payload, 1418mm reach, and simple programming.

Max Payload:
10 kg
Reach:
1418 mm
View CRX-10iA/L
Properlyworks logo
FANUC Authorized System Integrator

Properly Works

Properly Works is committed to helping customers overcome a wide range of manufacturing challenges related to productivity, costs, quality and recent issues driving personnel gaps in organizations.

Properly Works augments your existing manufacturing engineering team with experienced mechanical, electrical and automation resources to help improve your operations.

Visit Website https://properlyworks.com/
Seibel modern logo
End User

Seibel Modern

Since 1944, Seibel Modern has remained an industry leader in industrial welding and steel fabrication. The company has endured as a family-oriented corporation with over 60 employees in Lancaster, NY.

Visit Website