Skip to content Skip to navigation
Resources About MyPortal Login
Edit Entry
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
Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. First-Ever Robotic Paint Repair Solution on a Moving Automotive Line

First-Ever Robotic Paint Repair Solution on a Moving Automotive Line

GM improved paint finish consistency and reduced costs by automating top-coat inspection and repair using FANUC robots and 3M’s AI-driven system.

Solution By
3m logo
3M, Inovision
Published
January 15, 2025
Last Updated May 15, 2026
Share Facebook X LinkedIn Email Copied link
Image 121
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/first-ever-robotic-paint-repair-solution-on-a-moving-automotive-line

Results

Precision positioning

Unmatched moving line accuracy

Optimization 3

Greater consistency in finishes

Proven technology 3

Cost efficient

Image 121

Story

General Motors, like many automotive manufacturers, has traditionally relied on manual inspection of top-coat finishes. Using highly skilled operators, some of which may inspect up to 140 vehicles per shift, can create a number of challenges, including varying consistency in the finishes, inspection and repair, plus this type of manual labor can require a large footprint and high energy consumption.

To deliver the best ROI, an automated paint repair system would need to deliver consistent results while reducing production costs. Incorporating FANUC's reliable robots, 3M developed cutting-edge software, hardware, abrasives and compounds to create the 3M™ Finesse-it™ Paint Repair System. The system is a critical part of a complete automation solution that enables robots to efficiently and reliably sand and polish automotive finishes, making adjustments in real time on a moving line.

Inovision’s SMARTInspect™ system was developed to provide accurate and detailed information about paint inconsistencies in the manual or automated repair process. Together with 3M, Inovision initiated a joint development to robotically process the repairs and eliminate nearly all manual intervention. While 3M focused on developing sand and polish tools, dynamic process software, and a controller that utilizes stream motion to provide custom repair trajectories, Inovision was challenged with creating programs for the robots that position the tool 100mm above the vehicle surface, and within +/- 5mm of the area of concern. To achieve this level of accuracy, FANUC’s Karel programming language was utilized to control robot motion on the fly.

Because the production line was actively moving, Inovision engineers integrated technology to account for vehicle motion through the process. Plus, Inovision created software to manage the robotic line, which then seamlessly interfaced with the 3M Finesse-it Robotic Paint Repair System.

As a result of 3M and Inovision's work using FANUC robots, the automated system created a cost-efficient solution for GM that relies less on manual inspection and repair processes for a consistent finish every time.

"

Our partnership with 3M has resulted in a breakthrough technology for the field – the first ever Robotic Paint Finishing solution on a moving automotive line. Combining GM’s expertise in manufacturing and commitment to excellence with 3M’s deep technical knowledge of abrasives, software, hardware and application engineering experience, the once impossible is now possible. The difficulty to automate this process comes from each surface spot requiring a different recipe solution, in a different location of the car, while it’s moving on a line, every time. The 3M™ Finesse-it™ Robotic Paint Repair system delivers real time recipes and results for the ever-changing environment of the car moving on the line. This solution helps GM provide the highest level of quality to our customers.

Ryan Odegaard Director of Global Paint, Polymers & Additive Manufacturing – GM

FANUC Products Used

M-710iC/70
Articulated Robots

M-710iC/70

The FANUC M‑710iC/70 is a compact 6 axis robot suitable for various applications and combines a 70 kg payload with extremely high axis speeds.

Max Payload:
70 kg
Reach:
2050 mm
View M-710iC/70
3m logo
FANUC Authorized System Integrator

3M

3M (NYSE: MMM) believes science helps create a brighter world for everyone. By unlocking the power of people, ideas and science to reimagine what's possible, our global team uniquely addresses the opportunities and challenges of our customers, communities, and planet. Learn how we're working to improve lives and make what's next at 3M.com/news.

Visit Website https://www.3m.com/
FANUC Authorized System Integrator

Inovision

Inovision is a turnkey automation and robotics systems integrator specializing in automotive paintshop sealer, paint, and machine vision applications. Our patented paint defect inspection system employs AI and machine learning technologies to produce industry leading automated inspection accuracy. We provide expert engineering, controls, robot process, software development, and build services with a passion for the work and unending drive for customer satisfaction.

Visit Website https://www.inovision.com/
Gm logo
End User

General Motors

General Motors (NYSE:GM) is driving the future of transportation, leveraging advanced technology to build safer, smarter, and lower emission cars, trucks, and SUVs. GM’s Buick, Cadillac, Chevrolet, and GMC brands offer a broad portfolio of innovative gasoline-powered vehicles and the industry’s widest range of EVs, as we move to an all-electric future.

Visit Website