Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. High-Mix, Low Volume Prototype Shop Achieves Lights-Out Manufacturing with Robotic Automation

High-Mix, Low Volume Prototype Shop Achieves Lights-Out Manufacturing with Robotic Automation

KAD Models scaled high-mix prototyping with flexible FANUC automation, enabling lights-out CNC machining and rapid expansion from California to Vermont.

Solution By
Trinity Robotics Automation
Trinity Robotics Automation
Published
March 28, 2024
Last Updated October 30, 2026
Share Facebook X LinkedIn Email Copied link
Trinity Robotics Automation Video courtesy of Trinity Robotics Automation
A yellow FANUC robotic arm tending a blue MAXIA CNC machine, positioned between a parts storage rack and the machine’s control panel.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/high-mix-low-volume-prototype-shop-achieves-lights-out-manufacturing-with-robotic-automation

Challenges

01

Labor intensive, manual CNC loading requiring operators 24-7, which wasn’t cost effective for the small shop

02

Due to the high mix, low volume of parts needing CNC machining, prototyping shops typically don’t automate

03

The slow turnaround of production and prototyping was potentially causing companies to order elsewhere

Results

Proven technology 5

The automated machine tending expanded capacity and throughput by achieving “lights out” overnight production.

Product range 1

The FANUC M-710i/50 and R-1000/100F robots performing automated machine tending helped a small prototype operation to boost production.

Optimization 5

The machine tending automation helped shorten the turnaround and lead times.

A yellow FANUC robotic arm tending a blue MAXIA CNC machine, positioned between a parts storage rack and the machine’s control panel.

Story

KAD Models prototypes components for many industries including medical, consumer electronics, aerospace and automotive. The company began in Alameda, California and in 2019 expanded to Rudolph, Vermont. Even though prototyping and automation typically don’t appear together since prototyping involves such high-mix, low-volume part production, KAD Models CEO Brian Kippen saw automation differently when he opened his business’ second location in Vermont. He wanted an automation platform that would allow him to take unique part numbers and run them on a system that he likens to a “cafeteria” style where the automation doesn’t care what’s on a pallet. A few months later, Kippen contacted Trinity Robotics Automation, a FANUC Authorized System Integrator, to install two Trinity Automation AX cells.

KAD Models has two Trinity automation cells, the AX5 and the AX4. The AX5 uses a FANUC M-710iC/50 robot, which has 50 kg payload and 2050 mm reach, and the AX4 uses a FANUC R-1000/100F robot, which has a 100 kg payload and 2230 mm reach, tending a Matsuura 5-axis CNC machining center.

These systems provide a machine tending automation solution, but with a unique spin. Instead of the FANUC robot grabbing and loading an individual part via a work holding, operators load the parts into fixtures and those fixtures are loaded into the machine. From a list of programs in the CNC milling center, the operator selects a part number associated with the part that has been loaded. Next, the FANUC robot takes that part and puts it into a queue. When the milling machine is ready to run, it calls up a particular part and runs it via the automated system.

KAD Models’ programmers work during the day to prove out prototype parts, then set up the machines that run parts during the night. The automated cells can run all of them overnight into the next day without the need for a second or third shift. The programmers arrive in the morning and have all the completed parts waiting for them. Additionally, because the system doesn’t involve programming the FANUC robots, the solution is quickly implemented and easy for operators to learn.

The automation has allowed Kippen to rapidly set up his Vermont prototyping shop, allowing him to expand his business from the West Coast to the East Coast very quickly. Now, KAD Models is able to serve local manufacturers looking for specialized components.

Brian kippen
"

You can never replace the human hand. An automation system that is easily utilized and easily loaded allows you to take time during the day when everybody is available to do training. You think about lights out automation as an ability to free up the day, to focus on training, focus on setup.

Brian Kippen CEO & President – KAD Models

FANUC Products Used

M-710iC/50
Articulated Robots

M-710iC/50

The FANUC M‑710iC/50 is a compact 6 axis robot popular for machine tending, grinding, polishing, deburring, water jet cutting and washing applications.

Max Payload:
50 kg
Reach:
2050 mm
View M-710iC/50
R-1000iA/100F
Articulated Robots

R-1000iA/100F

The FANUC R‑1000iA/100F is a 6‑axis robot offering flexibility for demanding tasks and a wide range of high-speed spot-welding applications.

Max Payload:
100 kg
Reach:
2230 mm
View R-1000iA/100F
Trinity Robotics Automation
FANUC Authorized System Integrator

Trinity Robotics Automation

Trinity Robotics Automaton is focused on building and developing the most efficient, easy to use automated pallet systems for CNC machining centers.

Visit Website https://www.trinityautomation.com
Kad models logo
End User

KAD Models

KAD Models offers prototyping and production services including CNC machining, silicone molding and urethane casting in both Vermont and Alameda, California.

Visit Website