Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Robotic Metal Finishing Solution Automates a Challenging Manual Task

Robotic Metal Finishing Solution Automates a Challenging Manual Task

Charter Wire automated wire finishing with a FANUC robot to improve quality, reduce scrap, eliminate a hazardous task, and boost capacity.

Solution By
Acme Manufacturing Co
Acme Manufacturing Co
Published
November 7, 2024
Last Updated November 5, 2026
Share Facebook X LinkedIn Email Copied link
Acme Manufacturing Co Video courtesy of Acme Manufacturing Co
Image 108
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/robotic-metal-finishing-solution-automates-a-challenging-manual-task

Challenges

01

Employee safety

02

Labor challenges with turnover

03

Finish quality

Results

Young generation 2

Ability to take on more production work

Optimization 3

Quality of weld grind improved

Proven technology 3

Product rework was eliminated

Trending up 3

Scrap rate was reduced

Image 108

Story

Leading cold rolled and forming manufacturer, Charter Wire is a Tier 1 supplier of engineered shaped wire used in many industrial applications. The family-owned company was looking to automate a manual finishing process where operators removed welds using a handheld five-horsepower air grinder equipped with a coarse stone weighing a total of 30 pounds. This process took about five minutes and was one of the worst ergonomic exposures for Charter Wire employees, many refusing to work on the line and some even quitting because of it.

Charter Wire tapped FANUC ASI Acme Manufacturing to provide an automated robotic metal finishing solution. Acme used a FANUC R-2000iC/270F Robot to integrate a robotic material removal system grinding varying diameters of the steel wire, ranging from 0.90" to 1.75". A flash upset butt weld connects sections together with a large weld burr in the process.

As a result, Charter Wire is achieving a perfect finish every time and has successfully removed a dirty, dull and dangerous task from their manufacturing process. In addition to keeping their employees happy, the automation has helped the company lower scrap rates as well as enabled them to take on more business and meet the demand.

Michael oyervides
"

Acme using FANUC robots gave us a high degree of confidence that the robots were going to be able to stand up in our tough environment.

Michael Oyervides Services Manager – Charter Wire

FANUC Products Used

R2000i C 270 F Beauty Shot
Articulated Robots

R-2000iC/270F

The FANUC R‑2000iC/270F is a 6 axis heavy payload material handling robot with 270 kg payload, the strongest robot in the FANUC’s R‑2000 range of robots.

Max Payload:
300 kg
Reach:
2655 mm
View R-2000iC/270F
Acme Manufacturing Co
FANUC Authorized System Integrator

Acme Manufacturing Co

Acme has been providing quality tools to the metal finishing industry since 1910. This kind of longevity is unparalleled in the industry and has resulted in an industry-leading wealth of knowledge that makes Acme the preferred supplier across a broad spectrum of industries. Acme has a wide variety of applications within our core solutions that provide our customers with industry-leading technology.

Visit Website https://www.acmemfg.com
Charter wire logo
End User

Charter Wire

Founded in 1936 in Milwaukee, Wisconsin, Charter Wire has grown into a leading supplier and manufacturer of Engineered Shaped Wire, Cold Finished Bar, and Cold-Headed and Stamped Components to various industries including Automotive, Agriculture, Construction, Consumer, Industrial, and Oil & Gas. With two facilities in Milwaukee, we are well positioned to support our customers with cold rolling and forming manufacturing needs.

Visit Website