FANUC CNC Series 31i Model B5 Plus

CNC Grinder and Grinding Machine Solutions

FANUC CNC systems help CNC grinding machines and CNC grinders achieve precise abrasive motion, ultra-tight tolerances, smooth surface finishes and repeatable part quality.
A hand touching a computer screen Description automatically generated

CNC Grinding Solutions

CNC grinding is a precision finishing process that removes extremely small amounts of material from a part using a controlled abrasive wheel. In a CNC grinding machine, the CNC system manages wheel position, spindle speed, feed rate and machine movement so manufacturers can produce parts with tight tolerances, smooth finishes and precise geometries.

FANUC CNC systems are well suited for CNC grinder machines because they provide the speed, precision, repeatability and reliability required for demanding grinding applications. From surface grinding and cylindrical grinding to complex multi-axis grinding processes, FANUC controls help manufacturers improve accuracy, productivity and machine uptime.

Featured Products

FANUC CNC Controls for Grinding Applications

FANUC CNCs, known for their rock-solid reliability and unbeatable performance, enable grinding equipment to produce parts at a high rate with exceptional finishes. Thanks to our CNC’s ability to control very accurately the grinding wheel’s position, speed, feed and movement within microns, manufacturers can experience the full benefits of CNC grinding. The following FANUC controls are perfect for grinding applications.  

Four industrial CNC control panels side by side, each with a display screen, physical keypad, and numeric buttons; one unit includes a red emergency stop button.

30 Plus Series for CNC Grinding Machines

Take your machine tools to the next level with FANUC CNC Series 30i-B Plus, enhanced for 5-axis operations and faster cycle times. FANUC's Advanced CNC Series 30i/31i/32i-B Plus is our premium class of controls designed to maximize and simplify the operations of advanced machine tools.

Three black FANUC CNC control panels with keyboards, each displaying different screens including a machining status menu and a purple app-style home screen.

0iM-F Plus for CNC Grinding Machines

FANUC designed the 0i-MF Plus CNC Series to help machine shops achieve more efficient operations through optimizing spindle performance, reducing sequencing processing time and a customizable, user-friendly interface.

ROBODRILL Plus Technician Interacting With Series 31i MODEL B5 Plus CNC Panel
Applications

CNC Grinding Machine Applications

CNC grinding machines are used to produce parts that require exceptional accuracy, repeatability and surface quality. FANUC CNC systems support a wide range of CNC grinding applications, including:

  • Surface grinding
  • Cylindrical grinding
  • Tool and cutter grinding
  • Internal and external diameter grinding
  • Precision finishing
  • Multi-axis grinding
  • High-volume production grinding
  • Grinding for aerospace, automotive, medical device and general manufacturing parts
Benefits

Benefits of FANUC CNC Systems for CNC Grinding

CNC grinding performance depends on precise motion control, reliable machine operation and the ability to maintain consistent quality across demanding production runs. FANUC CNC systems help CNC grinding machines and CNC grinders achieve the speed, accuracy, repeatability and uptime required for precision manufacturing.

Global Automation Provider

FANUC started the development of Numeric Control (NC) technology back in 1955. Since then, our engineers have continuously engrained new and innovative technologies into our products. With over 60 years of experience and 40 million automation products installed worldwide, FANUC is a global leader in the automation industry. More CNC operators know and trust FANUC’s CNC platform.

High Performance

Based on high-speed, high-accuracy servo technology, FANUC’s CNC Systems maximize the performance of machine tools, such as improved productivity, high-speed, high-quality machining, and easy-to-use operability.

Reliability

FANUC CNC Systems are known for their rock-solid reliability. Our CNC products made in Japan are tested under strict conditions and designed to ensure consistent and long-lasting performance. This helps maximize machine tools’ uptime and optimize operations.

Easy to Use

FANUC CNCs can be easily customized to meet specific grinding requirements and come equipped with advanced features that make the system both user‑friendly and efficient. This flexibility and integration create the ideal combination for addressing the grinding industry’s unique needs.

Lifetime Support

FANUC’s philosophy of not terminating support of FANUC products for as long as they are used by our customers has made FANUC CNCs the most popular choice for machine tool users throughout the world. We are a Service First company, which means customer service is our highest priority.

Products

Products Related to Grinding

Type:
Industry:
FAQ

CNC Grinding FAQs

Learn what CNC grinding is, how CNC grinding machines work and how FANUC CNC systems support precision grinder machine applications.

CNC grinding is a precision machining process that uses computer numerical control to guide an abrasive grinding wheel as it removes small amounts of material from a workpiece. It is commonly used to achieve tight tolerances, smooth surface finishes and accurate part geometries.

FANUC CNC systems help CNC grinding machines control motion, speed, feed and positioning with high accuracy. This supports repeatable part quality, reliable machine operation, smooth surface finishes and productive grinding performance.

A CNC grinding machine is used to produce parts that require very tight tolerances, smooth finishes and repeatable accuracy. These machines are commonly used in aerospace, automotive, medical device, toolmaking and general manufacturing applications.