Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. A New Era of FANUC’s ROBODRILL Vertical Machining Center with More Offerings than Ever
ROBODRILL Plus α D28 Li B5 ADV Plus Y500 Monitor Graphic

A New Era of FANUC’s ROBODRILL Vertical Machining Center with More Offerings than Ever

The new FANUC ROBODRILL α-D28LiB5ADV Plus Y500 features a larger table, more tools, new capabilities, all in the same space-saving footprint.

Published
August 27, 2024
Reading Time
2 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (August 27, 2024) – FANUC America, a global industrial automation leader, unveils the latest addition to FANUC’s ROBODRILL vertical machining center (VMC) lineup, the new α-D28LiB5ADV Plus Y500. This new VMC offers more advantages to any production machine shop by featuring a larger table, shorter drilling and tapping cycles as well as more tools coupled with faster tool changes. FANUC America will be introducing the new ROBODRILL α-D28LiB5ADV Plus Y500 at the 2024 International Manufacturing Technology Show in Chicago, IL., Sept. 9-14 in booth S-338919.

FANUC’s ROBODRILL α-D28LiB5ADV Plus Y500 is designed for peak performance covering a wide range of tasks and excelling at machining large workpieces. This is due to its extended Y-axis stroke (500 mm) and increased table size, all without increasing the ROBODRILL’s footprint. The new ROBODRILL speeds up drilling and tapping operations via a rapid Z-axis acceleration (2.2 G) and traverse rate (60m/min). Plus, with an expanded tool capacity of 28 tools and lightning-fast changes, the new ROBODRILL α-D28LiB5ADV Plus Y500 will boost productivity for any machining application.

“We understand modern machine shops, particularly in the automotive industry, need to produce constantly, maximize machine time, and reduce any interruptions to production,” says Lou Finazzo, Vice President of FANUC America. “The new α-D28LiB5ADV Plus Y500 is built for reliable production, tailored to our customers’ needs for extra capabilities without sacrificing any floorspace.”

The enhanced performance of the new ROBODRILL α-D28LiB5ADV Plus Y500 is designed to help machine shops drive down cycle times with faster speeds and improved productivity. Additionally, with easy robotic integration tools with FANUC robots, automating machine tending is a breeze with FANUC ROBODRILL Plus.

This newest ROBODRILL Plus continues to build on ROBODRILL’s over 50-year reputation as the most reliable VMC with industry-leading uptime. The ROBODRILL Plus lineup offers precision and versatility with three model sizes available each in two choices: Standard or Advanced. With nearly a half million operating around the world, FANUC ROBODRILLs are popular for not only their performance, but 24/7 local support available to keep all machine shops running all the time.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.