Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC America Showcases Robot and Cobot Solutions at Pack Expo Chicago
Crx 20ia l bakery waterfall

FANUC America Showcases Robot and Cobot Solutions at Pack Expo Chicago

Global industrial automation leader FANUC America demonstrates its latest food-grade innovations for the packaging and processing industry in booth #N-5332.

Published
October 28, 2024
Reading Time
4 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (October 28, 2024) – FANUC America, a global industrial automation leader, will showcase its latest packaging and processing innovations at Pack Expo Chicago, in booth #N-5332. From food-grade cobots to stainless industrial robots, a wide range of agile solutions will demonstrate uninterrupted speed, reliability, accuracy and dexterity—all while maintaining food safety—in real-world applications.

Built with the highest quality standards, FANUC’s advanced automation technologies provide solutions to common industry challenges, including production, supply chain and labor shortages. Featured cobots and robots include:

  • Easy-to-use, food-grade CRX Collaborative Robots
  • High-speed and versatile SCARA Robots
  • FANUC DR-3iB/6 STAINLESS Food-Grade Delta Robot
  • The food-grade/cleanroom type, long-reach LR Mate 200iD/7LC robot

Picking, Packing and Palletizing Applications

Delivering reliability and accuracy that minimizes error, reduces product waste and enhances overall quality control, FANUC solutions will be shown in booth demonstrations that directly address common industry challenges.

Collaborative Robots

  • Food-Grade Cobot Bakery Tray Load and Unload with iRVision
    In this entirely new dual-cobot cell, attendees will see the controlled loading and unloading of cookies on bakery trays. Demonstrating its impressive 1,418 mm of reach, the FANUC CRX-20iA/L Food-Grade Cobot will use 3DV/400 iRVision mounted to its arm to locate and unload cookies from a tray and place them onto a conveyor, simulating a seamless cookie baking operation. A second CRX-20iA/L will then use a bakery tray to catch the cookies coming off the end of the conveyor and then place the now-full trays onto a cart.
  • Food-Grade Cobot Palletizing
    Shown for the first time at PACK EXPO, the FANUC CRX-30iA food-grade cobot—with a 30 kg payload and 1,756 mm of reach—will use PalletTool 3 software to efficiently palletize two pallets from a single infeed using a multi-case gripper.
  • Intuitive Cobot Programming
    In this kitting demonstration, attendees are able to use drag-and-drop icon based programming on the FANUC Tablet TP and three-button wrist to easily kit meat and cheese gift boxes with the CRX-10iA cobot. Ideal for those with little to no robotic experience, the cobot’s ease of programming is paired with FANUC’s world-renowned technology, proven reliability, and sensitive contact detection that allows the CRX-10iA to work safely alongside people.

Industrial Robots

  • High Speed Picking Application with Line Tracking Tools
    The DR-3iB/6 STAINLESS is FANUC’s first stainless steel food-grade delta robot for picking and packing primary food products, setting new benchmarks for payload, speed, reach and sanitation in robotic food handling. Using iRVision and iRPickTool line tracking software, this delta robot demonstration picks and places randomly oriented fish fillets alongside an SR-12iA/C, showcasing high speeds and product reorientation.
  • Food Assembly with Food-Grade Robots
    Offering a best-in-class work envelope for both upright and invert mount installations, the LR Mate 200iD series of tabletop industrial robots assembles cheeseburgers in this demonstration. Working alongside the SR-6iA/C will be the LR Mate 200iD/7LC – both food-grade/cleanroom robots – picking and placing buns, burgers and toppings before removing and reversing order so that the cycle can repeat.
  • Automated Palletizing and Depalletizing
    The six-axis M-710iD/50M robot, combined with two iRVision 3DV/1600 vision sensors and the FANUC iPC, will use the iPC’s AI Box Detection software to locate boxes within stock carts. Once located, the robot will depalletize boxes from one cart and utilize PalletTool to palletize them on the opposite cart. With one cart empty, the process will be repeated by depalletizing and palletizing back to the original cart. In this demo, tall stock carts highlight the advantage provided by the M-710i50-/50M’s curved arm. FANUC’s AI-driven iPC enables high-performance advanced picking in challenging lighting conditions to ensure seamless, reliable depalletizing.

Robotic Controllers

  • Powerful Performance with FANUC’s New Robot Controller
    Just announced, FANUC’s new R-50iA is the world’s* first robot controller to offer cyber security with a wide range of enhancements and new intelligent features designed to maximize robot performance. Attendees can learn about performance enhancements and optimized efficiency demonstrated in the heavy payload palletizing cell, which integrates the new robot controller.

Hear FANUC Experts

Session: How Standard Robotic Solutions Revolutionize Food Production
Panelists: Wes Garrett, Executive Director, Global Accounts, FANUC America;
and Chris Lorente, Executive Director, Global Accounts, FANUC America
Date: Sunday, Nov. 3, 2024 at 1:30 p.m.
Location: Innovation Stage 3 (N-4585)

Learn more: PACK EXPO Education


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.