Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. Fanuc Rechargeable Battery Unit Kit Provides Reliable Long-Term Backup Power for CNC Machines and Eliminates Use of Disposable Batteries

Fanuc Rechargeable Battery Unit Kit Provides Reliable Long-Term Backup Power for CNC Machines and Eliminates Use of Disposable Batteries

FANUC’s rechargeable battery unit provides long-term CNC backup power, eliminates disposable batteries, reduces downtime, and improves reliability and sustainability.

Published
August 15, 2013
Reading Time
2 min
Share Facebook X LinkedIn Email Copied link

HOFFMAN ESTATES, IL - (August 15, 2013) FANUC America Corporation – FANUC CNC now offers a Rechargeable Battery Unit Kit that provides reliable long-term backup power for CNC machines and eliminates the use of disposable batteries; providing a more environmentally-friendly solution.  As a result, there is no machine downtime due to dead batteries and no scrap parts due to loss of machine position.  The Rechargeable Battery Unit Kit removes the cost, hassle and inconvenient timing of replacing disposable batteries. 

FANUC’s Rechargeable Battery Unit enables one CNC system to be connected from a power source to the servo amplifiers, and it contains a rechargeable battery and charging circuit that supplies backup power to absolute pulsecoders and separate type detector units; thus eliminating the use of disposable batteries which is better for the environment.  

The charging circuit monitors the voltage of the rechargeable battery, and it charges the battery when the voltage becomes low. Because the charging circuit works only when it is necessary, the rechargeable battery can be used for a long period of time.  The average life span of the unit is more than 10 years, however working conditions or operating environment will affect life expectancy.

The kit includes all the necessary cables for one CNC system to be connected from a power source to the servo amplifiers and a connection manual. This kit is designed to be installed with Alpha, Alpha i or Beta i Servo Amplifiers and separate type detectors.

For aftermarket installation, customers can tap into the expertise of the FANUC Aftermarket Support Team that can do an audit of existing equipment to make configuration and installation recommendations for each specific application.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.