Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC Showcases CRX Cobots at The Battery Show North America
2022 Battery Show

FANUC Showcases CRX Cobots at The Battery Show North America

FANUC will demonstrate its popular line of CRX collaborative robots at The Battery Show North America in Novi, Mich., Sept. 13-15, booth #2626.

Published
August 26, 2022
Reading Time
2 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (Aug. 26, 2022) – FANUC, the global leader in CNCs, robotics and ROBOMACHINEs will demonstrate its popular line of CRX collaborative robots at The Battery Show North America in Novi, Mich., Sept. 13-15, booth #2626.    

FANUC’s CRX cobots are extremely robust and able to run for up to eight years without maintenance.  Interactive programming enables users to teach points using hand guidance or a tablet interface with drag and drop icons.  Following the success of the CRX-10iA and CRX-10iA/L, three new models were introduced this year including the CRX-5iA, CRX-20iA/L and CRX-25iA. The expanding cobot series can handle products from 5kg to 25kg and reach capabilities from 994mm to 1,889mm.   

There are now 11 FANUC CR and CRX cobot models available to help the battery, EV and other industries with production applications such as inspection, machine load/unload, packing, palletizing, sanding, welding, and many more.     

At the show, a FANUC CRX-10iA will provide attendees the opportunity to try the cobot’s intuitive hand guidance and easy-to-use tablet programming.  

In a second demonstration, a CRX-10iA/L will use AI Error Proofing to inspect for the presence/absence of components on steering wheels. FANUC’s AI Error Proofing is a function in iRVision® designed for part inspection that uses machine-learning technology.  The CRX-10iA/L equipped with a robot-mounted camera will inspect two steering wheels to determine passed or failed samples.  The steering wheels will be fixed to a table but can be rotated by an operator to show that the robot is able to inspect non-fixtured parts. 


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.