Contents
Food and beverage manufacturers are navigating a rapidly changing production environment. Labor shortages remain a challenge, product portfolios continue to expand, and rising costs are putting pressure on margins. At the same time, consumers expect more choices, leading to smaller production runs and more frequent packaging line changeovers.
To remain competitive, manufacturers need packaging operations that can adapt quickly while maintaining throughput, quality and efficiency. Flexible robotic automation is helping companies meet those demands by simplifying changeovers, improving consistency and creating a foundation for future growth.
Building Flexibility into Automation
Traditionally, automation projects were often viewed as complex investments that required extensive engineering and specialized programming skills. Today, advances in robotics, machine vision and software are making automation more accessible and adaptable.
Modern robotic systems can be configured to handle a wide range of package sizes, product formats and production requirements. Adjustable end-of-arm tooling allows robots to accommodate changing packaging needs, while machine vision systems enable robots to identify and pick products even when they are not perfectly positioned.
Software is also playing a larger role in flexibility. For example, FANUC's PalletTool3® software simplifies pallet pattern creation and modification, allowing operators to manage new products and changeovers through an intuitive interface rather than complex robot programming. Together, these capabilities help manufacturers respond to changing market demands without completely redesigning their production lines.
Flexibility in Action
The benefits of adaptable automation can be seen in the experience of Mrs. Gerry's, a prepared foods manufacturer that needed to increase production while managing labor constraints and frequent product changeovers.
The company relied on approximately 12 employees per shift to support its packaging operation and faced challenges related to product orientation, production bottlenecks and limited floor space. At the same time, the business needed additional throughput to keep pace with growing demand.
To address those challenges, Mrs. Gerry's implemented a modular packaging system that included robotic pouch orientation, automated case packing and robotic palletizing. The solution helped streamline packaging operations, reducing changeovers to approximately five to 10 minutes while supporting multiple product configurations within a limited footprint. Installed in just 10 days, the system achieved full production capacity and helped increase throughput to approximately 36 million pounds annually, providing the flexibility needed to support continued growth.
The project illustrates how modular robotic solutions can deliver meaningful improvements without lengthy installation periods or extensive disruption to operations.
Standardized Solutions Reduce Risk
For many manufacturers, standardized automation systems provide a practical starting point for robotics adoption.
Pre-engineered palletizing, case-packing and collaborative robotic solutions can reduce engineering requirements, accelerate deployment and simplify expansion across multiple lines or facilities. Because these systems are built on proven designs, they help lower implementation risk while allowing manufacturers to realize a return on investment more quickly.
This approach enables companies to start with a specific application and scale automation over time as business needs evolve.
Looking Ahead
As packaging requirements become more complex, manufacturers are increasingly looking for automation solutions that can adapt to new products, changing package formats and evolving production demands without requiring major system overhauls. Advances in robotics, software and automation technologies are making that level of flexibility more achievable than ever before. Emerging capabilities such as AI-enabled vision and natural language programming are helping make automation easier to install, operate and scale across manufacturing environments.
Whether through standardized robotic cells, scalable palletizing systems or AI-enhanced vision technologies, the most successful packaging operations will be those designed not just for today's requirements, but for whatever comes next.
For manufacturers evaluating automation, now is the time to identify packaging processes where changeovers, bottlenecks or operational complexity are limiting performance. Solutions designed with flexibility in mind can help address current production challenges while providing a foundation for future needs.