Skip to content Skip to navigation
Resources About MyPortal Login
Edit Entry
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
Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. MDS Enhances Efficiency and Quality with Robotic Welding Solution

MDS Enhances Efficiency and Quality with Robotic Welding Solution

MDS Manufacturing boosted output, improved weld quality, and reduced lead times by up to 30% using Acieta’s FastARC robotic welding with FANUC.

Published
April 18, 2024
Last Updated September 11, 2026
Share Facebook X LinkedIn Email Copied link
Acieta LLC Video courtesy of Acieta LLC
A yellow Acieta welding robot arm performing arc welding on a metal fixture, producing bright sparks, within a red-framed industrial work cell.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/mds-enhances-efficiency-and-quality-with-robotic-welding-solution

Challenges

01

Increase production speed

02

Alleviate manual welders from mundane tasks

03

Improve quality

04

Forecast lead times

Results

Proven technology 6

Enables time studies to accurately forecast production.

Product range 1

Reduced rework/higher quality.

Young generation 4

Allows employees to focus on projects that require higher skills.

Optimization 5

20-50% efficiency improvement.

A yellow Acieta welding robot arm performing arc welding on a metal fixture, producing bright sparks, within a red-framed industrial work cell.

Story

MDS Manufacturing is a leading industrial equipment supplier based in Parkston, SD. MDS specializes in loader attachments including buckets, grapples, hay tools, and pallet forks for all the major tractor brands.

Producing many similar types of parts, MDS typically had one person welding the same parts all day long. With increasing business, MDS knew they needed a better way to weld repeatable parts more quickly and efficiently with less rework. In 2023, they realized they needed to implement robotics, but were apprehensive because they had never used automation before. Once they met with the engineering team at Acieta – everything fell into place. After evaluating the operation, Acieta recommended their FastARC® robotic welding cell which includes a FANUC Arc Mate robot. FastARC is a standard pre-engineered robotic arc welding cell and is ideal for companies adopting automation for the first time. The cell’s small footprint and easy installation, combined with Acieta’s operator training, helped MDS get started right away.

The robotic work cell has enabled MDS to streamline production by consolidating multiple operations into one single operation with the robot. For example, before the automation it took about 16 hours to weld 100 parts. Now, it takes the robot just 13 hours to do the same number of parts, which is a 30 percent reduction in operating time for just that one part.

Employees are excited to work with the robot cell, which relieves them from mundane tasks and allows them to focus on projects that require higher skills.

According to MDS management, the FastARC cell has not only met but exceeded performance expectations. This achievement is marked by improved consistency and reduced rework. Additionally, with the implementation of the robot cell, MDS can now generate more accurate time studies and forecast lead times effectively. As a result, they are better equipped to swiftly fulfill customer orders.

Looking ahead, MDS is considering additional automation based on the 20-50 percent efficiency gains they have experienced with the FastARC robotic welding cell. When the time comes, they intend to collaborate with Acieta, leveraging their engineering expertise and excellent customer support.

Alec hohn quote
"

With the robot, we didn't replace any of our workers, we just minimized the mundane tasks, which allowed them to focus on the bigger projects and what's considered more fun.

Alec Hohn Engineer – MDS

FANUC Products Used

FANUC ArcMate 100iD robotic welding arm in yellow, equipped with a Lincoln Electric AutoDrive wire feeder and MIG welding torch
Arc Welding

ARC Mate 100iD/8L

Long-arm arc welding robot ideally suited for working in compact robotic cells where extra reach is required for welding.

Max Payload:
8 kg
Reach:
2032 mm
View ARC Mate 100iD/8L
Mds
End User

MDS

MDS Manufacturing Company Inc. is a third generation, family-owned company that has been serving the agricultural community for over 40 years. Their continuing commitment to agriculture and dedication to produce top quality products has made MDS a leader in the manufacturing of skid steer, tractor loader, telehandler, and wheel loader attachments for most major brands of equipment in North America.

Visit Website