Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC America Demonstrates Automated Solutions for Welding and Painting at FABTECH
IMG 2389

FANUC America Demonstrates Automated Solutions for Welding and Painting at FABTECH

FANUC America will demonstrate a variety of robots, cobots, and industrial automation solutions at FABTECH 2024, October 15-17, in Orlando.

Published
October 2, 2024
Reading Time
4 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (October 2, 2024) – FANUC, a global industrial automation leader, will showcase the latest automation technologies for the fabrication industry at FABTECH 2024, Oct. 15-17, in Orlando. From collaborative robots that can weld safely alongside humans to the world’s first explosion-proof paint cobot, innovative and easy-to-use robotics will demonstrate real-world applications in FANUC America booths.

  • In Main Booth #W-4817, attendees can find a variety of FANUC’s robot and cobot welding and laser solutions, from precision welding to high-speed laser cutting.
  • In Paint Booth #W-2729, attendees will see various demonstrations, including the brand-new CRX Paint Cobot, which delivers flawless results – whether in automotive coatings or intricate designs – while offering precision, flexibility and easy operation.

All-new demonstrations include two innovative collaborative robot welding applications, in addition to the FABTECH debut of the FANUC M-950iA industrial robot showcasing high rigidity and precision via friction-stir welding.

Innovations in Welding Automation

Easy-to-use CRX cobots offer the same accuracy and repeatability as all FANUC robots, with the added benefit of simple programming, the ability to work safely and in close proximity to humans. At FABTECH, attendees will find a variety of FANUC collaborative robot demonstrations, including:

  • Flexibility and Efficiency: Welding near human operators requires flexibility as well as efficiency, demonstrated by the CRX-10iA/L cobot—mounted on an integrated 7th robot transfer unit (RTU)—which simulates ARC welding at one station while an operator loads the second station.
  • Drop Center Positioning: Showcasing the impressively long 1,889 mm reach of the new CRX-30iA/L cobot, an ARC welding demonstration of a skid steer cab on an integrated auxiliary axis showcases ease in handling large components.
  • Easy Programming: An all-new FANUC programming interface with buttons on the wrist allows welders with little to no robotic experience to create programs easily, as evidenced by the CRX-10iA/L cobot—with a 10 kg payload and 1,418 mm reach—in a live welding demonstration.
  • Rigid Precision: Making its FABTECH debut, the M-950iA/500 heavyweight robot features a wider range of motion, offering an impressive 500 kg payload capacity and 2,830 mm reach, showcased in a new friction stir welding demonstration featuring a StirRob Friction Stir Welding Head by FPT Industrie.
  • High-Speed Laser Cutting: The new M-800/60-20B, FANUC’s next-gen, high-accuracy industrial robot, will showcase high-speed laser cutting, connected to a TRUMPF TRUFiber 4001 P and LaserMech FiberCUT STa. Cut holes are generated with Shape Gen software for easy single point teaching.

New Automated Robotic Painting Solutions

FANUC’s Paint Booth will highlight the benefits of robotic painting solutions for operations of all sizes and needs. With the industry’s widest range of paint robots that increase production and keep workers safe, we’ll be showing our latest innovative products for the painting, powder and/or gel coating with fiberglass reinforcement industries, including:

  • The New Paint Cobot, Now Available: As the first explosion-proof collaborative paint robot available globally, the CRX-10iA/L Paint unlocks the benefits of flexible automation for more companies, including high-mix, low volume operations. Be sure to see it in action at the show!
  • Cobot Inspection for Paint: To help ensure a perfect finish every time, the CRX-10iA/L will demonstrate its ability to perform detailed color matching inspection tasks even in the smallest of spaces.
  • Visual Tracking for Boosting Production: We’ll be featuring a FANUC P-40iA paint robot using iRVision 3DV and the new Visual Tracking for PaintTool software to quickly and reliably track and paint randomly oriented parts. Working in tandem, a CRX-20iA using iRPickTOOL and iRVision software will load/unload guitars.
  • Versatile Paint Automation: Highlighting how FANUC paint robots are perfect for automating the painting of smaller and more challenging parts, the P-40iA paint robot will use coordinated motion with a turntable to precisely paint plastic automotive pieces.

Factory Automation and IoT

In the main FANUC booth, we’ll display the latest FANUC CNC products that enable machine tool builders to go to market with the best equipment possible. Our demos will highlight our powerful and energy efficient new Alpha i-D Servo System as well as our dedicated CNCs for laser cutting machines.

For operations looking for shopfloor connectivity solutions, we’ll be showcasing our IoT station featuring MT-Link i, which provides real-time equipment status as well as critical production and maintenance info to fuel data-driven business decisions.

FANUC experts will participate in several conference sessions at FABTECH.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.