Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC America Highlights Latest Intelligent Automation Solutions at ATX West
IMG 9413

FANUC America Highlights Latest Intelligent Automation Solutions at ATX West

FANUC will highlight its latest factory automation products and a variety of intelligent robot and cobot solutions at ATX West in Anaheim, CA, Feb. 7-9, in Booth #4500.

Published
January 5, 2023
Reading Time
4 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (Jan. 5, 2023) – FANUC, the global leader in CNCs, robotics and ROBOMACHINEs will highlight its latest factory automation products and a variety of intelligent robot and cobot solutions for assembly, vision-guided material handling, machine tending and more at ATX West in Anaheim, CA, Feb. 7-9, in Booth #4500.

FANUC’s Latest Factory Automation

  • Industrial PCs for All Needs: FANUC offers industrial PCs providing a powerful platform for custom developments in a wide variety of applications. Available in several different sizes and options, FANUC’s industrial PCs are fast, secure and easy to use.
  • The FANUC Digital Servo Adapter-Model B is a motion control device that enables the integration of a FANUC servo system with an existing, third-party control.
  • For machine shops looking to take advantage of IoT data, MT-Link i provides real-time equipment status and conditions info as well as other important production and maintenance data.

CRX Cobot Demonstrations

FANUC’s expanded series of CRX collaborative robots are extremely robust and can run for eight years without maintenance. Easy-to-use interactive programming enables users to teach points using hand guidance or a Tablet TP with drag and drop icons.  

Machine Tending - A CRX-10iA/L with FANUC QSSR (Quick & Simple Start-up of Robotization) will demonstrate how easy it is to connect a FANUC CRX cobot and a machine tool.   QSSR simplifies the automation of machine tool load/unload applications using the CNC controller’s easy guidance functionality for quick connectivity, start-up and operation. 

Palletizing - A CRX-25iA robot, offering a 25kg payload and 1,889mm reach will demonstrate case palletizing.  Guided by a 3DV/200 iRVision® sensor mounted to the arm, the CRX-25iA will palletize boxes to nearly 7’ high. In addition, the CRX-25iA will be mounted to a mobile cart to showcase its flexibility.  The robot can be easily repositioned by hand and uses vision to automatically adjust to its new location and continue working accurately.

Packing - A CRX-10iA will demonstrate packing health and beauty products.  Attendees can try the cobot’s intuitive hand guidance and easy-to-use Tablet TP programming.   

FANUC SCARA Robots

FANUC recently expanded its line of four-axis SCARA robots to include the SR-3iA/U ceiling mount featuring a full 360-degree work envelope with no dead zones, the robot can access any point within its reach.  In addition, FANUC’s SCARA lineup also includes the SR-3iA/C and SR-6iA/C cleanroom variants.   

High-Speed Tracking Demonstration - The SR-3iA/U ceiling mount SCARA robot has a 3kg payload and 350 mm reach. The SR-3iA/U will use iRVision 3DV and iRPickTool to pick various parts from a moving circular conveyor, move them to a 2D camera for inspection, then place them onto an outfeed conveyor into the appropriate Pass/Fail locations.

Breakfast Sandwich Assembly - SR-6iA/C and LR Mate 200iD/7LC Robots

An LR Mate 200iD/7LC and SR-6iA/C – both cleanroom robots - will assemble four breakfast sandwiches.  First, the LR Mate 200iD/7LC uses iRVision 3D to pick and place a bun on a plate.  At the same time, the SR-6iA/C SCARA robot will pick and place a sausage patty on top of the bun. This continues until patties are placed on all four buns.  The robots will alternate placing the remaining elements on each sandwich including an egg, a slice of cheese and a top bun. Once all four sandwiches are completed, the robots remove items in reverse order and the cycle repeats. 

Visual Line Tracking – LR Mate 200iD/7L Robot

A FANUC LR Mate 200iD/7L uses an overhead mounted 3DV/400 Vision Sensor to find and track parts moving down a conveyor. The robot picks a part and places it into a bin. The system highlights the speed and accuracy of the 3DV/400 vision sensor and the ability to detect the 3D orientation of a work piece.

Built-in Intelligence

FANUC offers application software for packaging and palletizing, integrated iRVision® and tracking features, ROBOGUIDE simulation, Dual Check Safety (DCS), and Zero Down Time (ZDT) to help customers monitor and manage their automation.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.