Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. Fanuc Introduces FASBacCNC Powerful & Easy To Use Network Based Backup Solution for CNC Files

Fanuc Introduces FASBacCNC Powerful & Easy To Use Network Based Backup Solution for CNC Files

FANUC’s FASBacCNC provides secure, automated CNC file backups, reducing downtime risk and ensuring reliable data protection across networked machines.

Published
January 26, 2015
Reading Time
2 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (January 26, 2015) FANUC America Corporation introduces FASBacCNC (FOCAS Automation Solution Backup CNC), a powerful and easy to use network based backup solution for FANUC CNCs. FASBacCNC eliminates the risk of one of the most common and expensive service interventions - extended downtime as a result of the loss of critical files on the CNC following a hardware failure or operational mistake. 

FASBacCNC provides peace of mind by automatically backing up the CNC files that have been created and customized by the machine tool builder or end user to a remote network server. Files backed up can include CNC parameters, PMC ladder and parameters, custom macros and variables, part programs, tool offsets and workpiece coordinate system offsets.

FASBacCNC is a front end application that interfaces with FANUC’s FASConnect server for file browsing, scheduling and backup operations for FOCAS enabled FANUC CNCs. FASBacCNC can work with multiple FASConnect servers across an entire network, so that files from a single machine, work cell, factory or even multiple factories can be combined into a single configuration for backup scheduling. FASBacCNC can be used on any personal computer on the network located out in the factory, back in an office or from a remote location.

Users browse their FASConnect servers with easy to use drag & drop navigation. Individual files can be uploaded manually or multiple files from multiple CNCs across the network can be included in a configuration. Multiple configurations can then be combined into a single scheduled backup. Powerful and flexible scheduling allows automatic backup to be executed hourly, daily, weekly or monthly. Users may also execute schedules manually for immediate needs.  Users receive email notifications relating to the scheduled backup status.

FASBacCNC is the latest addition to the FAS (FOCAS Automation Solution) lineup.  The complete FAS (FOCAS Automation Solution) suite includes:  FASBacCNC – a user interface for FASConnect allows browsing of all FASConnect servers and backup data either manually or on a scheduled basis, FASConnect - a Windows® service allows access and management of text data from all FOCAS enabled CNCs across a network, FASOPC - an OPC 3.0 compliant server for easy retrieval of machining data from all FOCAS enabled CNCs. 


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.