Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Freres Engineered Wood Boosts Throughput and Quality with FANUC Robots

Freres Engineered Wood Boosts Throughput and Quality with FANUC Robots

Freres Engineered Wood doubled Mass Ply Panel production and improved joint quality using FANUC robots integrated by PRE-TEC.

Solution By
Pre Tec, A Division Of Willamette Valley Company
Pre Tec, A Division Of Willamette Valley Company
Published
July 11, 2023
Last Updated November 13, 2026
Share Facebook X LinkedIn Email Copied link
Pre Tec, A Division Of Willamette Valley Company Video courtesy of Pre Tec, A Division Of Willamette Valley Company
A yellow FANUC R-2000iC robotic arm lifting a wood panel with a clamp gripper in a plywood manufacturing facility, with stacked panels in the foreground and a conveyor line beside it.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/freres-engineered-wood-boosts-throughput-and-quality-with-fanuc-robots

Challenges

01

Panels’ joint quality varied, which can comprise performance

02

Equipment setup was difficult and time-consuming, tying up manpower and equipment

03

Panel vibration could cause extra wood to be cut off panel edges, also reducing joint performance

04

Needed a flexible automation solution instead of custom designed equipment for cost competitiveness

Results

Proven technology 8

Robots improved quality by creating better joints and controlling vibration, which creates correctly cut panel edges 

Product range 3

Less complications in input panel process to free up manpower and equipment

Quality improvement 2

Higher percentage of their product meets or exceeds Quality Control (QC) requirements

Maintenance health 1

Predictable maintenance with robots’ monitoring and reporting software ZDT and service cycle

Optimization 6

Gained production capacity and throughput via extended hours beyond a normal shift

A yellow FANUC R-2000iC robotic arm lifting a wood panel with a clamp gripper in a plywood manufacturing facility, with stacked panels in the foreground and a conveyor line beside it.

Story

Located in Oregon, Freres Engineered Wood produces Mass Ply Panel, a lumber-based structural panel used as an alternative for concrete and steel in multi-story construction projects. This sustainable building material has been used in Europe for decades and is now growing in popularity in the US.

Freres wanted to boost production efficiency and improve the quality of their panels via better joints—key to the panels’ strength. Since both ends of the panel were being cut independently by different heads at the same time, matching the cut to both ends of the panel was extremely difficult. Additionally, panels were often bowed or cupped, which adversely affected the profile of the scarf joint. Finally, panel vibration could not be adequately controlled potentially causing the cutting heads to remove extra wood from the panel edge, which subsequently compromised joint performance.

By adding FANUC R-2000iC/210L robots integrated by FANUC Authorized System Integrator PRE-TEC, each end of the panel is now positioned by the robot to the same cutting edge to ensure both joints are balanced. This has significantly improved the quality of the panels’ joints, which boosts their strength and performance. Moreover, the automated cutting system has doubled production capacity because two robots now continually feed the same cutting head. This helps optimize the manpower and floor equipment to support growth in future demand.

Kyle freres vp of freres
"

We're really looking at technology and robotics in particular as a way to support the innovation that our industry needs to survive and our company in particular, to survive for another hundred years.

Kyle Freres Vice President of Operations – Freres Engineered Wood

FANUC Products Used

R 2000i C 210 L Beauty Shot Right
Articulated Robots

R-2000iC/210L

Equipped with 6 axes for ultimate flexibility, the FANUC R‑2000iC/210L robot is capable of handling heavy loads precisely within a generous work envelope

Max Payload:
210 kg
Reach:
3100 mm
View R-2000iC/210L
Pre Tec, A Division Of Willamette Valley Company
FANUC Authorized System Integrator

Pre Tec, A Division Of Willamette Valley Company

PRE-TEC is a leading automation systems integrator specializing in turnkey material handling solutions. Designed systems combine multi-axis robot arms, custom end-of-arm tooling, conveyance systems, and safety hardware to address, resolve and optimize the most challenging manufacturing applications.

Visit Website https://www.pre-tec.com/
Freres logo
End User

Freres Engineered Wood

What began 100 years ago as one man with his horses, Charlie and Trixie, has since grown into Oregon’s premier producer of veneer and engineered wood products for the commercial construction industry.

Visit Website