Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC Demonstrates Easy to Use Cobots at Amazon’s re:MARS Conference

FANUC Demonstrates Easy to Use Cobots at Amazon’s re:MARS Conference

See FANUC at Amazon’s re:MARS Tech Showcase where we’ll demonstrate how easy it is to program and use a FANUC cobot.

Published
May 30, 2019
Reading Time
2 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (May 30, 2019) – FANUC America, the leading supplier of robotics, CNCs and ROBOMACHINEs has expanded its line of easy to use collaborative robots to include six models. Look for FANUC at Amazon’s re:MARS Tech Showcase (June 4-7 in Las Vegas) where we’ll demonstrate how easy it is to program and use a FANUC CR-7iA collaborative robot.

FANUC’s series of power and force limiting collaborative robots can handle 4-35 kg payloads and a 550-1813 mm reach. Easy to program and use – even for those with little or no experience - FANUC’s cobots are equipped with FANUC’s iHMI intuitive touch screen user interface that includes step-by-step programming instructions right from the teach pendant. Simple and straightforward programming helps reduce costs associated with operator training, minimizes setup time and increases system productivity. In addition, FANUC’s Hand Guidance feature allows operators to teach a collaborative robot by leading it through paths at the press of a button and/or use it to lift heavy objects manually. 

FANUC’s six cobot models combine world-renowned automation technology, proven reliability and very sensitive built-in sensors that allow them to work safely alongside people in a variety of industrial/manufacturing jobs including machine tending, dispensing, inspection, kitting, palletizing, e-commerce, and more. In addition, FANUC’s collaborative robots are equipped with intelligent options such as iRVision® and force sensing. 

“We offer the industry’s widest range of collaborative robots in terms of payload, reach and speed options,” said Amanda Nixon, collaborative robot product manager, FANUC America.  “In addition, our cobots are very easy to program with FANUC’s Hand Guidance or the iHMI touch screen, and provide easy plug-and-play for intelligent options like vision and force sensing. No other cobot brand in the world can offer what FANUC provides to our customers, including lifetime product support.”


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.