HandlingPRO Intro Plus (ROBOGUIDE)
Course code: PRO0310-2
- Length
- 2 days
- Classroom hours
- 16
2-day ROBOGUIDE training for application engineers covering workcell design, simulation, cycle time studies, CAD path generation, and robot coordination.
See course dates and enroll. A FANUC Academy login is required to register.
Target Audience: This course is designed for application engineers who need to design robotic workcells, perform cycle time, reachability studies, or generate robot paths.
Prerequisites: Completion of a live or virtual FANUC instructor-led HandlingTool Operations and Programming course. Completion of an online HandlingTool eLearn will not meet this prerequisite. The student needs to be familiar with teach pendant menus, jogging, frames, positional information, basic programming, and fault recovery of the robot prior to attendance in this class. Students who have attended a class more than four years in the past are required to pass a preparatory test prior to attending the class. Students must be able to log into the Academy URL while in class, to access learning materials.
Course Objectives: Understand the difference between a real and virtual teach pendant. Jog the robot using alternative methods to the traditional teach pendant method Add and define parts, fixtures, and EOAT for the purpose of picking and placing Setup an extended axis as well as additional motion groups Create and modify programs with the simulation editor and program generator using CAD to path analyze Program execution with the Task Profiler Understand different methods for matching a real workcell to a virtual workcell Understand how to coordinate the motion between two robots using I/O interconnect
This course consists of lectures, chapter reviews, demonstrations, and a series of lab exercises designed to reinforce what the student has learned. In addition to lab exercises, a pre-test and a post-test are used to measure mastery of objectives.
Dress Code: Appropriate business casual attire is required to attend any class at all FANUC training facilities. No shorts, leggings, tank tops, or open-toe shoes are permitted. PPE: Is not required for this class.
Drop/Rescheduling Policies. with any questions.
Prerequisites
Training Path
-
FANUC Robotics Training Path
The recommended order for FANUC robot training, from operator basics through advanced programming, vision and maintenance.
Where This Course Is Offered
Products Covered in This Course
Advanced Operation and Programming in Japanese
This is an advanced programming class that follows Basic operation and programming. It covers advanced programming techniques, DCS functions, and much more. This material is suitable for those who have mastered basic operations to step up to the next level.
HandlingPRO Intro Plus (ROBOGUIDE)(Virtual)
3‑day virtual HandlingPRO/ROBOGUIDE training covering workcell simulation, cycle time analysis, CAD path generation, robot coordination, and validation.
Advanced Teach Pendant Programming R-50iA Controller
5‑day Advanced Teach Pendant Programming training for R‑50iA controllers covering offsets, collision guard, background logic, I/O, payload setup, and automation.
Advanced TPP Programming R-30iA, R-30iB, R-30iB Plus
5‑day virtual advanced robot programming training covering offsets, collision guard, background logic, I/O, payload setup, and production automation.