Contents
Heavy Work Needs Smart Movement
Manual lifting can quickly exhaust an individual, regardless of the shift. Repetitive tasks involving weight, reach or twisting pressure impede productivity and contribute to injuries, delays and inconsistent product handling.
A mechanical arm offers a solution. A cobot arm operates continuously, repeating the same pattern, grip and path with precision. Its performance remains consistent, unaffected by fatigue.
Early cobot arm systems typically required substantial space and full caging. However, contemporary cobot arm designs have revolutionized this. Modern controlled machines operate safely alongside human workers, achieve tighter tolerances and execute clean patterns without the need for constant recalibration.
The key advancement lies in superior control. This has been achieved through force-limiting joints, smooth axis movement and more sophisticated motion profiles.
Factories that once rotated workers hourly now rotate finished parts every few seconds, a testament to the transformative impact of a cobot arm.
Grip, Grab, Repeat: How the Modern Gripper Works
A cobot end-of-arm-tool (EOAT) completes repetitive motion with accuracy, adjusts to varying part shapes and keeps pace with production without drifting off pattern. Whether placing circuit boards, transferring cartons or gripping irregular parts, the right gripper turns a mechanical arm into a controlled, dependable tool.
Servo electric grippers give you full control over speed, position and force — and when paired with FANUC CRX cobots, they’re plug-and-play. The DH Servo Electric Gripper integrates directly into the CRX control system without extra wiring or complex programming. It supports variable grip settings, handles fragile parts without damage and maintains performance across different product runs. This precision becomes especially useful for electronics, medical packaging and high-mix lines where grip variation matters.
On the other end of the spectrum, vacuum grippers like the COVAL CVGC series use lightweight carbon bodies and foam or suction cup interfaces to grip cardboard, sheet goods or finished packaging. Built for compatibility with CRX cobots, the CVGC supports easy setup, easily-readable controls and a modular plate system that adapts to box size or shape. Whether the job involves palletizing, machine loading or kit preparation, this gripper series adds strength without slowing down the cobot.
Smaller footprints benefit from mini grippers that tuck into tight machines or assembly nests. Parallel or concentric grippers offer reliability where rugged contact is expected. A cobot fitted with this kind of tooling gives more control in overhead operations.
FANUC’s EOAT lineup supports grippers, tools and sensors to match any of these needs. Explore Grippers and find the right combination for your part geometry, cell layout and throughput targets.
Power and Force Limited Arms That Keep Going
A Power and Force Limited arm starts with motion that responds to real-time force feedback data. Servo motors move each axis with specific torque, speed, and direction settings. Force sensors measure external contact force and compliance during contact with the part. Together, these systems create smooth, exact motion that stays consistent over thousands of cycles.
A robot arm designed with this level of control prevents drift, slip or stutter during movements. It creates seamless transitions between pick-and-place operations, even when subjected to various defined loads. This is particularly important with production lines that operate at maximum speed, as every lost second directly impacts output. Smooth motion maintains a consistent product flow, minimizes tool wear, and optimizes takt time throughout the shift.
FANUC has specialized in servo control since the beginning. The company’s background in CNC shaped its servo architecture, which now powers millions of cobots and CNCs around the world. A mechanical arm built with this heritage doesn't need constant correction.
FANUC CRX collaborative cobots take this further. They bring precise motion into open environments without the need for cages or physical barriers. Safety-rated torque limits, collision detection, and cycle memory all work together to maintain uptime.
Vision + Cobots Together
A vision-guided cobot integrates visual and kinetic capabilities into a singular system. It executes picking, placing or inspecting tasks with real-time feedback, removing reliance on static coordinates. Consequently, the cobot can adapt instantaneously, tracking minor part displacements, verifying alignment and preventing erroneous grabs.
Vision-guided systems enhance precision throughout every operational phase. A cobot and end effector integrated with vision can locate irregular components within a bin or precisely center a label prior to application. A cobot with a servo-electric tool is capable of sorting disparate products by size, color or orientation without requiring a change in tooling. Each of these movements is predicated upon the camera's input, rather than pre-programmed estimations.
FANUC iRVision® uses plug-n-play software and hardware with the cobot and controller to maintain ease of use. No third-party sensors, extra wiring, or long configuration time. Setup happens faster and stays stable even as production demands change. Whether it’s packaging, assembly or inspection, pairing a vision system with the cobot raises accuracy, lowers rejection rates, and keeps the cell efficient.
Small Footprint, Big Output
A cobot doesn't need a wide footprint to make a big impact. In high-mix environments with limited space, cobots can handle repetitive, weight-bearing tasks right beside operators without crowding the floor. That’s where compact systems with strong lifting power make the biggest difference.
Sorting, palletizing, and bin picking often involve tight conveyor turns or confined loading zones. Whether you have long gripper fingers or a vacuum end effector, you don’t sacrifice control, grip strength, or speed repeatability.
The FANUC CRX-30iA fits into this category with a 30 kg payload, a 1756 mm reach, and a mechanical weight of only 135 kg. Its wrist-mounted buttons make direct teaching easier and allow quick, flexible programming without stepping away from the arm. That kind of built-in usability turns high-lift jobs into low-stress tasks for smaller teams.
Built to Stay on the Line
A robot arm that runs every shift needs torque and reach, but it also needs staying power. Downtime slows the whole operation, and constant maintenance pulls resources from other priorities. That’s where durability and service make the difference.
Cobot arm design at FANUC focuses on lifetime performance. Every model, from large-payload machines to compact cobots, is built to operate for years under real production pressure. Motors, cables, joints and control systems all work together to keep motion smooth and failure rates low, even in high-duty cycles.
Support doesn’t end after installation. FANUC’s Zero Down Time (ZDT) software gives smart alerts before breakdowns happen, using usage data and diagnostic trends to flag service needs early. Combined with 24/7 technical support and guaranteed parts availability, that means less time offline and fewer surprise repairs.
FANUC backs every cobot for life. Learn more about Service First to see how long-term support protects long-term output.
No Two Arms Are the Same
The selection of a cobot manipulator necessitates careful consideration of the specific task requirements. Different product lines demand varying attributes, such as extended reach, precise wrist rotation or delicate handling capabilities. Grip strength and payload capacity are equally crucial, particularly when dealing with diverse materials or fragile packaging.
For instance, a pneumatic parallel gripper would be unsuitable for soft-tissue packaging, just as a servo electric gripper would be inadequate for loading engine blocks. Cobot end effectors must be aligned with the characteristics of the object being manipulated, the required operational speed, and the spatial constraints of the environment. Factors such as payload, end-of-arm tooling, and motion profile are all significant considerations.
Whether the application calls for a six-axis collaborative cobot with a broad operational range or a compact manipulator designed for exact bin placement, the robot selection process commences with an analysis of the product itself. Aligning the motion capabilities with the demands of the job ensures optimal performance.
Why Cobots Now Carry the Weight
Cobots have moved beyond small tasks. A cobot can now load, stack, pick, inspect and reset for the next cycle without hesitation or error. Each move comes from a cobot arm design built for repeat performance and it keeps going without strain, shift after shift.
FANUC CRX cobots use the same footprint to handle loads up to 30 kg and adjust to low-volume, high-mix production without changeover delays. A cobot can lift weight with precision to keep the line moving and allow the operators to work safely beside the system.
FANUC's extensive range of cobots provides options for industries of all kinds. Exploring our product offerings and consulting with experts can help you identify the perfect solution for your needs. Get in touch with us today.