Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Robotic Automation Speeds Up Lion Electric’s EV Battery Production

Robotic Automation Speeds Up Lion Electric’s EV Battery Production

MJC Engineering beat supply delays with FANUC America, delivering a precision CNC spinning machine on time for hydrogen storage and clean energy applications.

Published
September 26, 2023
Last Updated October 22, 2026
Share Facebook X LinkedIn Email Copied link
Video courtesy of JR Automation
Two yellow FANUC articulated robot arms working in a clear-paneled automation cell with aluminum framing, handling flat panel components near a conveyor and shelving system.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/robotic-automation-speeds-up-lion-electrics-ev-battery-production

Challenges

01

Lion needed to produce their own battery to have better control of their supply chain.

02

Minimal time to create a product prototype and scale up the production process.

03

Needed a cost-effective solution.

Results

Proven technology 7

Lion Electric and JR Automation developed a cohesive team that tackled the project as one unit working towards the same goals.

Product range 3

In a matter of months, the team scaled up the system to deliver a fully automated solution.

Quality improvement 2

The system is a prime example of JR Automation's ability to design complex, large-scale systems for its customers.

Two yellow FANUC articulated robot arms working in a clear-paneled automation cell with aluminum framing, handling flat panel components near a conveyor and shelving system.

Story

According to Lion Electric, in the EV space, there’s a big advantage to producing your own battery, which is the most expensive component in an electric vehicle.

In a traditional product launch, companies create and perfect a product prototype before implementing or revising the manufacturing system. However, with minimal time to get up and running, Lion Electric needed the product design and battery production process to be on point as quickly as possible to meet customer demands.

The collaborative relationship with JR Automation, a Hitachi Group Company, allowed both teams to work closely together to achieve their goals quickly. While the Lion team worked on the development of battery components, the JR team was able to flag and identify any potential obstacles that could happen in production. This process allowed JR’s engineers to gain a better understanding of the types of materials required for the application, along with dispensing and other techniques related to battery production. The result was a highly effective and safe automated battery production process.

The system includes a variety of FANUC robots and other automation equipment that will be an integral part of Lion Electric's new production facility. The automated system enables Lion to scale production and keep operating costs at a manageable level.

Screenshot 2025 09 03 at 11 27 06 AM
"

We had to get the product right, the process right, and the suppliers right on the first try, it was fantastic working with the JR team.

Diego Castro Battery Plant General Manager – Lion Electric

FANUC Products Used

M-10iD/12
Articulated Robots

M-10iD/12

The FANUC M‑10iD/12 is a compact 6 axis robot that reaches the highest axis speed and precision in its class.

Max Payload:
12 kg
Reach:
1441 mm
View M-10iD/12
M-900iB/400L
Articulated Robots

M-900iB/400L

The FANUC M‑900iB/400L is a long arm 6 axis heavy payload robot with 400 kg payload for processes requiring heavy-weight handling within a wider work envelope.

Max Payload:
400 kg
Reach:
3704 mm
View M-900iB/400L
R-2000iC/125L
Articulated Robots

R-2000iC/125L

Equipped with 6 axes for ultimate flexibility, the FANUC R‑2000iC/125L robot is capable of handling heavy loads precisely within a generous work envelope

Max Payload:
125 kg
Reach:
3100 mm
View R-2000iC/125L
Yellow FANUC industrial M-20iB/25 robotic arm on a dark base, shown against a white background with its multi-jointed arm extended upward and to the left.
Articulated Robots

M-20iB/25

The FANUC M‑20iB/25 is a compact 6 axis robot that has been designed to achieve faster cycles and increased throughput on a range of applications.

Max Payload:
25 kg
Reach:
1853 mm
View M-20iB/25
Lion electric logo
End User

Lion Electric Co.

The Lion Electric Co. is an innovative manufacturer of zero-emission vehicles. Lion designs and manufactures all-electric school buses, midi/minibuses for special needs or urban transit as well as urban trucks. Lion is a leading OEM in transportation electrification in North America. Lion’s capabilities include the design, manufacture, and assembly of many of their vehicles’ components, including chassis, battery packs, cabin and powertrain.

Visit Website