FANUC America’s advanced troubleshooting and service specialists for unique CNC situations.
Specialized CNC Service: Customer Application Support Team (CAST)
FANUC embraces a culture of “Service First,” which means customer service is our highest priority. We are committed to supporting FANUC products for the lifetime of their use and to achieve this, all of FANUC America’s Service technicians are dedicated and knowledgeable about FANUC products. However, there are occasional situations that require a much more in-depth response. For these special occurrences, FANUC America’s Customer Application Support Team is ready to assist.
What is the Customer Application Support Team?
This is a specialized team that provides an advanced level of support to customers that go beyond the standard Field Service activities. They provide application support for various items such as servo optimization, ladder/PLC programming, data collection and help add new features to an existing product installation. They can also help add functionality to a machine no longer supported by the industry.
Who are Customer Application Support Team members?
The Customer Application Team is the advanced level of Field Service support made up of engineers that have a broader range of skills when it comes to all FANUC CNC products. All members are senior engineers of the Field Service team.
Where are FANUC America’s Customer Application Support Team members located?
Our engineers are located throughout the country and support all customers located in the United States, Puerto Rico & Canada.
Do I need to specifically ask for a Customer Application Support Team member?
No, customers might not even know that they need the Customer Application Support Team and occasionally a standard service call might be escalated to a member. Regular CNC assistance requests should be made through the FANUC America Technical Support Call Center, available 24/7 at 1-888-FANUC-US (1-888-326-8287 (phone prompts 2 & 2). From there, the Service team will route the call to the Customer Application Support Team if deemed necessary.
What are some of the specialized services the Customer Application Support Team performs?
Listed below are some of the many advanced Field Service options available. Please contact FANUC Service for a quote and to determine if your machine qualifies for these services. In addition, other tasks that require assistance can be quoted upon request.
IOT - Install and support:
MT-LINKi – Monitor operational and production data
FASOPC – Easy retrieval of machining data from all FOCAS enabled CNCs
FASConnect – Access and management of text data from all FOCAS enabled CNCs
Manual Guide i - Installations, setup and basic training
Scale Configuration- Parameter configuration for new scale installations