Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC Demonstrates a Variety of Robot and Cobot Solutions at the Assembly Show
Screenshot 2025 08 27 at 11 48 03 AM

FANUC Demonstrates a Variety of Robot and Cobot Solutions at the Assembly Show

FANUC America will demonstrate a variety of robot and cobot solutions at The Assembly Show, Oct. 26-28, in Rosemont, IL in booth #731.

Published
October 4, 2021
Reading Time
5 min
Share Facebook X LinkedIn Email Copied link

ROCHESTER HILLS, MI – (Oct 4, 2021) – FANUC America, the leading supplier of CNCs, robotics, and ROBOMACHINEs will demonstrate a variety of robot and cobot solutions at The Assembly Show, Oct. 26-28, in Rosemont, IL in booth #731.  

High-Speed SCARA Robot Solutions

FANUC’s family of 4-axis SCARA robots has grown to include the SR-3iA, SR-6iA, SR-12iA, and new SR-20iA models with 3kg, 6kg, 12kg and 20kg payload capacities, and a 400mm - 1100mm reach, respectively. FANUC’s SCARA robots are designed to help customers increase productivity in a number of industries including consumer goods, batteries and other auto components, plastics, lab automation, appliances and medical devices.

The small SR-3iA and SR-6iA SCARAs have a compact footprint and space-saving design for maximum efficiency.   In addition, the SR-3iA/H and SR-6iA/H are 3-axis variants that provide strong performance and an affordable alternative to small linear slide products.  The higher-payload SR-12iA and SR-20iA robots provide flexibility with a large vertical stroke, and an Environmental Option for harsh conditions.  All of FANUC’s SCARA robots provide excellent robot motion, speed and precision.

Powered by the R-30iB Compact Plus controller, FANUC’s SCARAs have the same intelligence and reliability that’s available on all FANUC robots, including integrated iRVision®, conveyor tracking (iRPickTool), and most other software options.  FANUC’s SCARA iRProgrammer user interface makes it easy to setup and program the robot on a Tablet or PC (Teach Pendant is optional).

At the show, FANUC’s latest SR-20iA SCARA robot will assemble battery packs with screws. The demonstration shows the SR-20iA’s ability to handle heavy parts in a wide operating area at high speeds.

In a second SCARA demonstration, a FANUC SR-3iA picks randomly oriented parts from a moving circular disc and places them onto a conveyor at high speeds. Visual Circular Tracking combined with FANUC iRVision and iRPickTool software enables the robot to quickly track, locate, pick and place the parts with the highest precision.   

CRX Collaborative Robot  

FANUC’s CRX cobot is an easy-to-use and flexible solution for a variety of applications, including inspection, palletizing, packing, welding and more.   Built-in sensors on each axis can allow the CRX cobot to work safely alongside people without the need for expensive guarding.  In addition, the CRX can operate for eight years maintenance-free, which is a game-changer for companies looking to lower costs and maximize productivity.

At the show, a FANUC CRX-10iA/L equipped with an iRVision 3DV/200 vision sensor will demonstrate case palletizing.  The CRX will use the 3DV sensor to find a box, pick it up from one pallet and place it on another pallet.  

In addition, a FANUC CRX-10iA/L collaborative robot will use a robot-mounted iRVision camera to inspect or error proof multiple areas of two steering wheels.  The CRX robot will position the camera over different sections of the steering wheels while iRVision’s AI Error Proofing tool determines if the inspection passes or fails.  The AI Error Proofing tool will check to verify the presence/absence of components on the steering wheels. 

A third CRX cobot will be available for visitors to try its easy hand guidance and tablet programming features. 

The CRX collaborative robot offers the same high level of performance that all FANUC products are known for including the latest technologies and world-renowned reliability.  It supports several of FANUC’s advanced features including iRVision, and is a perfect fit for any application where collaborative robots can help customers achieve higher efficiencies.  Also, interactive programming enables users to teach points using hand guidance or a new tablet interface with drag and drop icons.

Medical Device Assembly Featuring the FANUC LR Mate 200iD Robot

An LR Mate 200iD/7C robot, ideal for clean room and food environments will assemble small electronic medical devices (fingertip pulse oximeters).  First, the robot uses iRVision to pick plastic top covers and place them onto the bottom housing in an assembly fixture.  A robot-mounted FANUC FS-15iA force sensor is used to push and pull the assembly as a quality check.  Once the devices are assembled, the parts are disassembled and the process repeats. 

The popular LR Mate 200iD series of tabletop industrial robots offer a “best in class” work envelope for both upright and invert mount installations. Ten models include clean room and wash proof versions, each with various wrist speeds and reaches to accommodate even the most limited workspace.  Since the LR Mate series was launched nearly 30 years ago, it has become one of FANUC’s biggest sellers, with over 70,000 units installed across the globe. 

FANUC will participate in two technology workshops including:

WORKSHOP #1 | How Robotics Are Helping the EV Market Grow at a Rapid Pace on Tuesday, October 26, 10:30 – 11:00 AM.  Rob Kuphal Director of Sales - Automotive Corporate Accounts.   FANUC America to present: Growing Infrastructure Will Require Massive Amounts of Automation.

WORKSHOP #3 | Robotics Assembly – Beyond the Basics on Tuesday, October 26, 1:35-2:10 PM. Josh Person, Staff Engineer at FANUC America to present:  Vision Guidance for Robotic Assembly.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.