Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  5. FANUC Demonstrates Robot and Cobot Solutions for Picking, Packing and Palletizing at Pack Expo
IMG 5281

FANUC Demonstrates Robot and Cobot Solutions for Picking, Packing and Palletizing at Pack Expo

See FANUC America's latest robot and cobot solutions at Pack Expo Chicago, Oct. 23-26 in booth #N6116.

Published
September 27, 2022
Reading Time
9 min
Share Facebook X LinkedIn Email Copied link

Rochester Hills, MI – (Oct. 11, 2022) – FANUC America, the global leader in CNCs, robotics, and ROBOMACHINEs will highlight its latest robot and cobot solutions for picking, packing and palletizing at Pack Expo Chicago, an exhibition for automated picking, packing, palletizing and more, Oct. 23-26 in booth #N6116.

New: FANUC DR-3iB/6 Stainless Delta Robot Handling Protein

At Pack Expo, the DR-3iB/6 STAINLESS delta robot will use 3DV iRVision® and iRPickTool line tracking software to pick randomly oriented pieces of chicken from a continuous infeed conveyor. Equipped with a Soft Robotics gripper, the robot picks chicken breasts and reorients them onto an outfeed conveyor. The cell features high-speed automated picking with product re-orientation.

“The DR-3iB/6 Stainless is FANUC’s stainless steel food-grade delta robot for picking and packing primary foods,” said Jessica Juhasz, staff engineer, FANUC America. “With an IP69K rating, the robot meets USDA and FDA food safety standards, which will help companies increase their production efficiencies without compromising food safety.”

The DR-3iB/6 STAINLESS features a fully enclosed stainless steel body that is resistant to the chemicals and high pressure/temperatures required in strict wash-down environments. It has a 1200mm reach (450mm height) and a powerful four-axis design allowing it to handle 6kg payloads at high speeds. The robot’s mirror-like surface finish ensures that any microbial contaminants can be washed away cleanly. With additional features such as NSF H1 food-grade lubricant, secondary oil catch basins (with viewing windows to monitor potential leaks), self-draining surfaces and many other small details driven by USDA/FDA standards, the DR-3iB/6 STAINLESS delta robot is ideally suited for primary food handling applications.

The new robot operates with FANUC’s latest R-30iB Plus controller with integrated intelligent functions such as iRVision, Force Sensing, Robot Link, Collision Guard and Zero Down Time (ZDT).

“We’re showcasing the many features of the DR-3iB/6 STAINLESS that makes it stand out in terms of payload, speed, reach and sanitation,” added Juhasz.

CRX Cobot Demonstrations

Earlier this year, FANUC expanded its popular series of CRX collaborative robots with the new CRX-5iA, CRX-20iA/L and CRX-25iA. The CRX cobots are extremely robust and able to run for eight years without maintenance. Easy-to-use interactive programming enables users to teach points using hand guidance or a tablet interface with drag-and-drop icons. The new CRX cobots complement FANUC’s existing line of CR and CRX cobots that now total 11 model variations able to handle products from 4 to 35kg.

Palletizing

A new CRX-25iA robot, offering a 25kg payload and 1,889mm reach will demonstrate case palletizing. Guided by a 3DV/200 vision sensor mounted to the arm, the CRX-25iA will palletize boxes to nearly 7’ high. In addition, the CRX-25iA will be mounted to a mobile cart to showcase its flexibility.

The robot can be easily repositioned by hand and uses vision to automatically adjust to its new location and continue working accurately.

Loading Storage Carts

The new CRX-20iA/L cobot equipped with a 3DV/200 vision sensor will pick consumer items of varying sizes and shapes that weigh up to 20kg and load them onto a storage cart. The demonstration highlights the cobot’s wide motion range and ability to handle large and heavy packages, relieving workers from physically demanding jobs.

Packing

A CRX-10iA will demonstrate packing health and beauty products. Attendees are invited to try the cobot’s intuitive hand guidance and easy-to-use tablet programming.

New M-10iD/12 Food-Grade Variant Robot: Rice Bag Packaging

FANUC will demonstrate its new Food-Grade M-10iD/12 robot picking bags of rice off dual conveyors and packing them into a box. The demonstration highlights the robot’s speed and flexibility to handle various payloads.

With the release of two new Food-Grade variants, the M-10iD/12 and the larger M-20iD/25, FANUC has further expanded its offerings for customers in the food industry that need high-speed and high-payload robots. Both units feature food-grade oil on all axes, stainless steel wrist flanges, motor covers, corrosion-resistant fasteners, white epoxy paint and the Severe Dust & Liquid Protection package.

In addition to the new M-10iD/12 and M-20iD/25 Food-Grade variants, the M-10iD and M-20iD robot series include six additional compact material handling robots - the M-10iD/12, M-10iD/10L, M-10iD/8L, M-10iD/16S, M-20iD/35, and M-20iD/12L. Rated best-in-class for speed and repeatability, the M-10iD and M-20iD robots offer a sleek and lightweight design and feature hollow wrists/J3 axes. A curved J2 robot arm minimizes interference with work pieces and fixtures. The robots’ payload capabilities range from 8-35kg, allowing them to handle a wide variety of products. Also, a long reach (1103mm to 2272mm) and stroke – even in the backflip region – makes it easier for customers to apply the robots while maximizing their available workspace – including larger parts or tooling.

Extra environmental protections such as FoundryPRO are available on select robots, and the M-10iD/12 can also be configured with a Dustproof Wrist Cover.

LR Mate 200iD/7LC and SR-6iA/C Robots: Breakfast Sandwich Assembly

The new SR-3iA/C has a 3kg payload and 400mm reach. It features a white epoxy coating and is rated IP54, meaning it is protected against contamination from limited amounts of dust and other particles as well as water spray. The SR-3iA/C is rated ISO Class 5 for cleanroom operation and uses NSF-H1 food-grade grease and anti-rust bolts for food handling applications.

An LR Mate 200iD/7LC and SR-6iA/C – both cleanroom robots - will assemble four breakfast sandwiches. First, the LR Mate 200iD/7LC uses iRVision 3D to pick and place a bun on a plate. At the same time, the SR-6iA/C SCARA robot will pick and place a sausage patty on top of the bun. This continues until patties are placed on all four buns. The robots will alternate placing the remaining elements on each sandwich including an egg, a slice of cheese and a top bun. Once all four sandwiches are completed, the robots remove items in reverse order and the cycle repeats.

The popular LR Mate 200iD series of tabletop industrial robots offer a “best in class” work envelope for both upright and inverted mount installations. Ten models include clean room and wash-proof versions, each with various wrist speeds and reaches to accommodate even the most limited workspace.The LR Mate series was introduced 30 years ago, and since that time has become one of FANUC’s most popular robot models with over 70,000 units installed globally.

The new SR-6iA/C has a 6kg payload and 650 mm reach. It features a white epoxy coating and is rated IP54, meaning it is protected against contamination from limited amounts of dust and other particles as well as water spray. The SR-6iA/C is rated ISO Class 5 for cleanroom operation and uses NSF-H1 food-grade grease and anti-rust bolts for food handling applications.

NEW FANUC LR-10iA/10 Robot: Vision-Guided Each Picking

A new FANUC LR-10iA/10 robot, guided by several 3DV/400 vision sensors mounted over the workcell, will pick various combinations of products from four separate totes to demonstrate order fulfillment. When the order tote is completed, it moves to the opposite side of the cell, where an LR Mate 200iD robot picks and places each item back onto the conveyor, sorting them by color to refill the pick totes.

FANUC’s LR-10iA/10 robot is designed for machine tending and many picking applications found in the warehousing and logistics markets.  Weighing just 46 kg, the LR-10iA/10 robot mounts to the floor, upside down, or on an angle. It’s also very easy to mount the robot to an AGV or other mobile platform.

SR-12iA SCARA Robot: Packing and Unpacking

The SR-12iA SCARA Environmental Option robot will pack and unpack four-packs of two-liter pop bottles. The demonstration shows the SR-12iA’s ability to handle heavy products in a wide operating area at high speeds.

FANUC recently expanded its line of four-axis SCARA robots to include the SR-3iA/U ceiling mount featuring a full 360-degree work envelope with no dead zones, and the SR-3iA/C and SR-6iA/C cleanroom variants. In addition to the three new models, FANUC’s series of 4-axis SCARA robots includes the SR-3iA, SR-6iA, SR-12iA, and SR-20iA with 3kg, 6kg, 12kg and 20kg payload capacities, and a 400-1,100mm reach, respectively. The higher-payload SR-12iA and SR-20iA SCARAs each offer a large vertical stroke and an IP65 environmental option for harsh conditions.

FANUC M-410iC/110 Palletizing/Depalletizing with Tablet TP Unit Load Creation

The M-410iC/110 robot will alternate between picking cases from two conveyors and palletizing a mixed layer unit load to depalletizing the product from the pallet back to the two conveyors. While the system is running, visitors can create their own custom unit loads from FANUC’s Tablet TP. The demonstration shows how easy it is to create and modify unit loads directly from the Tablet TP with FANUC’s PalletTool Turbo software using the newly updated user interface. This will give operators the ability to quickly modify their system without needing a computer with PalletPRO simulation software.

The M-410iC/110 robot is designed for high-volume case, bag and bottle palletizing operations. It features a 110 kg payload, four-axis articulation, a compact footprint, and a slim arm with through-arm cable routing to simplify dress-out and minimize interference with tooling and other peripheral devices. The ability to perform 2200 standard palletizing cycles an hour with a 60kg payload makes the M-410iC/110 the fastest palletizing robot in its class. It also features a compact footprint and a 646 mm interference radius, ideal for tight workspaces.

FANUC’s Impact on Pack Expo Chicago

FANUC’s expo robot displays, particularly in terms of automated picking and delta robot technology, showcase our ongoing dedication to enhancing industrial efficiency and reliability. The event highlights our latest advancements and sets the stage for future developments in robotic automation, cementing FANUC's role as a key player in this ever-evolving industry.


About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan and provides industry-leading CNC systems, robotics, and ROBOMACHINEs. FANUC’s innovative technologies help manufacturers maximize productivity, reliability, and profitability. Headquartered in Rochester Hills, Michigan, FANUC America has facilities throughout North and South America. Learn more at www.fanucamerica.com or explore collaborative robots at crx.fanucamerica.com.