SR 9i A R Circular Line Tracking Closeup 2

IMTS 2026

Visit FANUC America at IMTS, booth 338900 September 14-19, 2026 at McCormick Place, Chicago.
IMTS2026
Date
Location
Chicago, IL
Booth
338900
Share Facebook X LinkedIn Email

See FANUC America at IMTS 2026

Achieve the impossible at IMTS 2026. IMTS 2026 will be held September 14-19, 2026 at McCormick Place, Chicago. Manufacturers achieve the impossible at IMTS by pushing the boundaries of innovation, forming lasting connections, and discovering advancements redefining manufacturing.

Visit FANUC America at IMTS, booth 338900. We look forward to seeing you at the show!

Ready to Get Started?

Tell us about your project and a FANUC specialist will be in touch.

Name
Address

This site is protected by reCAPTCHA and the Google Privacy Policy and Terms of Service apply.

Demonstrations

See What’s Possible in Manufacturing Automation

Explore live demonstrations spanning collaborative and industrial robotics, Physical AI, machine tending, welding, assembly, vision, painting, machining and more. See how FANUC technologies can help manufacturers solve complex production challenges, improve flexibility and take productivity to the next level.

CRX 3i A Vertical Up Welding 1 2
CRX-3iA

Vertical Up Welding​​

Watch the portable CRX‑3iA sense its mounting angle and produce controlled vertical-up welds using easy-to-program triangular weaving.

Explore the CRX-3iA
CRX 20i A L Dynamic Line Tracking Inbolt Closeup 1
CRX-20iA/L

Tracking and Bolt Tightening​

Powered by Physical AI and Inbolt, the CRX-20iA/L tracks moving parts in real time and precisely tightens bolts to the desired torque while in motion.

Explore the CRX-20iA/L
FANUC R-2000/225F-27E and R-2000/210F-31 E robots performing spot welding
R-2000/E Series

Multi-Robot Spot Welding

See two R‑2000/E robots coordinate panel handling and fixtureless spot welding with integrated servo gun control and no external panels.

Explore the R-2000/E Series
FANUC P 55 15 21 A R50 Controller
P-55/15-21A

Paint Robot with Line Tracking​

See the P‑55/15 – 21A track moving helmets for precise painting, supported by the new R‑50iA compact cabinet with an integrated purge system.

Explore the P-55/15-21A
SR 9i A R Circular Line Tracking Closeup 1
SR-9iA/R

Circular Line Tracking

See the SR‑9iA/R use 3D vision to track and inspect spark plugs, then switch grippers to load trays and pack boxes automatically.

Explore the SR-9iA/R
M-810 Wet Machining
M-810/190-20B

Wet Machining​

See the M‑810/190 – 20B bring CNC-controlled flexibility to wet machining, performing rough milling, drilling, grinding and part handling.

Explore the M-810/190-20B
FANUC ROBODRILL Closeup
ROBODRILL

New ROBOMACHINE Products

IMTS 2026 will mark the debut of FANUC's next-generation ROBODRILL DC Series machining centers featuring FANUC’s latest CNC and servo technologies:

  • The D54CS performs heavy drilling, high-speed drilling and tapping on S50C steel with the 10k high torque spindle paired with Smart Spindle Load Control
  • The D74CS performs high-speed cutting capabilities with the new 12k high-acceleration spindle, showcasing the latest in software functions and G-codes exclusive to ROBODRILL for cycle-time reduction
  • The D116CS introduces the expansion of the X-Axis stroke to 1100 mm and Y-Axis to 600 mm; using the high-inertia DDR-TiB, FANUC performs high-precision positioning and high-speed processing of large electric vehicle instrument panels
At IMTS 2026

Advancing the Future of Manufacturing

From intelligent robotics and collaborative automation to virtual factory simulation and AI-driven production, FANUC is helping manufacturers solve today's challenges while preparing for tomorrow's opportunities. Discover the technologies shaping the next generation of manufacturing at IMTS 2026.

Physical AI

Physical AI

FANUC is collaborating with NVIDIA to advance Physical AI—a new paradigm that merges artificial intelligence with physical robotics to enable machines that see, reason, and act in dynamic environments. This approach empowers manufacturers to create photorealistic digital twins of their factories, train robots virtually, and deploy them with unprecedented speed and flexibility.

Cobots and robots

Cobots & Robots

From high-speed robotic welding and wet machining to flexible cobot inspection and kitting, our solutions are built to be fast to deploy, easy to use, and engineered to boost productivity and profitability across the automotive sector.

Smart digital twin

FANUC's Smart Digital Twin for Manufacturing

FANUC's Smart Digital Twin offerings help optimize your processes for faster, better and more accurate machining. Digital twins provide virtualization of the machine, control and machining processes. Digitalizing real-world applications makes operations more efficient by proving out CNC machining in the virtual world. That means less waste, better quality and more production.

Location

McCormick Place

McCormick Place
Loading map...