Desafíos
Seasonal labor shortages during peak harvest periods
Repetitive manual palletizing of heavy boxes led to worker fatigue and injury risk
Production bottlenecks caused by manual handling operations
Limited floor space on certain lines
Resultados
Eliminated repetitive heavy lifting and reduced ergonomic injury risks
Improved production flow, consistency and throughput
Automated a 4-person manual operation and redeployed employees to higher-value roles
Increased workforce satisfaction by removing physically demanding tasks
Implemented more than six robotic systems, with additional automation projects planned
Historia
Founded in 2007 and based in Stockton, California, Pearl Crop is a family-owned food processing company specializing in nuts, seeds and food ingredients. As a third-generation family business, the company provides a wide range of processing services, including roasting, seasoning, nut butter production and packaging.
Each year, Pearl Crop processes more than 100 million pounds of nuts and seeds. Yet, while demand remains steady throughout the year, nearly all harvested product arrives within a concentrated harvest window lasting only a few months. This seasonal surge creates unique operational challenges, particularly when it comes to staffing labor-intensive production processes.
One of Pearl Crop's biggest challenges was finding and retaining workers for repetitive palletizing tasks. Employees were required to repeatedly lift and stack boxes weighing between 25 and 50 pounds throughout entire shifts. The work was physically demanding, created potential ergonomic risks and often led to production bottlenecks during periods of peak volume.
Recognizing that labor constraints would limit future growth, Pearl Crop began exploring automation as a way to increase throughput, improve consistency and create a safer work environment.
The company found an ideal partner in RentoRobot, a robotics provider focused on flexible automation deployment models. Rather than requiring a significant upfront capital investment, RentoRobot offered a rental-based approach that allowed Pearl Crop to quickly implement automation, evaluate performance and scale deployments as needed. The partnership succeeded because Rent-A-Robot approached the project much like Pearl Crop approaches its own customers: by first understanding operational pain points, production requirements and business goals before recommending a solution.
Working closely with Pearl Crop, RentoRobot deployed FANUC robotic systems tailored to the company's different production environments. For applications where floor space was limited and production speeds were moderate, the FANUC CRX collaborative robot proved to be an ideal solution. Its compact footprint and ease of deployment allowed the system to be moved between production lines while providing automated pick-and-place and palletizing capabilities. The collaborative design also provided flexibility for operations where employees and automation needed to work in close proximity.
For higher-volume applications requiring faster cycle times and heavier lifting, RentoRobot implemented a FANUC R-2000 industrial robot. Designed to handle demanding palletizing operations, the robot enabled Pearl Crop to automate the movement of 50-pound boxes at production speeds that would be difficult to maintain manually.
The impact was immediate. Automated palletizing improved consistency and production flow while eliminating repetitive lifting tasks that previously placed strain on employees. In one operation line, a process that had traditionally required four workers became fully automated. Rather than eliminating jobs, Pearl Crop reassigned those employees to other roles where they could contribute more value and develop new skills.
Employee response to the automation has been overwhelmingly positive. Workers no longer spend entire shifts bending, stretching, lifting and stacking heavy boxes. Instead, they can focus on more skilled operational tasks while the robots handle the repetitive, physically demanding work.
Today, Pearl Crop has deployed more than six robotic systems across its operation, with additional automation projects already planned. The increased throughput and operational efficiency created by automation have enabled the company to focus greater attention on innovation, customer needs and future growth.
Productos FANUC Utilizados
CRX-30iA
El CRX-30iA es un robot de gran capacidad de carga de hasta 30 kg, que incorpora botones en la muñeca para una programación y personalización directa y sencilla
- Max Payload:
- 30 kg
- Reach:
- 1889 mm
M-410iC/185
El FANUC M‑410iC/185 es un robot compacto de paletización de 4 ejes para aplicaciones de paletización, ensamblaje, mecanizado y transferencia alta velocidad.
- Max Payload:
- 185 kg
- Reach:
- 3140 mm
R-2000iC/125L
El FANUC R‑2000iC/125L, con 6 ejes, manipula cargas pesadas con precisión y máxima flexibilidad en un amplio espacio de trabajo.
- Max Payload:
- 125 kg
- Reach:
- 3100 mm